We are using the MPC 860 power pc QUICC processor we are using the code warrior IDE for debugging . While entering into the debug we are getting an error as below .Find the below attachment for the CCS log.
Thank you
Best regards
Maheshwar
Test CCS connection to your board using the following commands in CCS console:
(bin) 49 % config cc cwtap
(bin) 50 % show cc
The following commands also can be used:
(bin) 49 % log v
(bin) 50 % source IDcode.tcl
Is there connection to the CodeWarrior TAP and MPC860 if these commands are used?
Have a great day,
Pavel Chubakov
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------