Is there a place I can download old version of processor expert?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Is there a place I can download old version of processor expert?

1,031 次查看
marcdrouin
Contributor I

I need to do a small modification to a customer project that have been build using processor expert 10.0.

When trying to open PE project with processor expert 10.4 it is like a blank project, only processor and flash.

So I expect that if I can use the version 10.0 it may work better... but I can't find a link to older version on NXP site.

Any help will be greatly appreciated.

Marc

标记 (1)
0 项奖励
回复
1 回复

937 次查看
BlackNight
NXP Employee
NXP Employee

Hi Mark,

the .pe files have been very compatible (I never had an issue with switching versions back and forward).

Are you sure it is 'Processor Expert 10.0'? Or are you talking about CodeWarrior for MCU 10.0 (which includes Processor Expert)? Can you tell what IDE you are using? And if you can, post your .pe file and I can have a look if it is really a problem of the file or something else.

I hope this helps,

Erich

0 项奖励
回复