I have been evaluating the M54455EVB. I want to use the M54452 processor in a embedded system. I have been trying to get the Ethernet (FEC) to work on the M54455EVB but no success yet. Is there any sample code for the Ethernet FEC? If yes, where can I dow

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I have been evaluating the M54455EVB. I want to use the M54452 processor in a embedded system. I have been trying to get the Ethernet (FEC) to work on the M54455EVB but no success yet. Is there any sample code for the Ethernet FEC? If yes, where can I dow

726件の閲覧回数
johnchan
Contributor I

I have been evaluating the M54455EVB. I want to use the M54452 processor in a embedded system.

I have been trying to get the Ethernet (FEC) to work on the M54455EVB but no success yet.

Is there any sample code for the Ethernet FEC? If yes, where can I download the sample code?

ラベル(1)
0 件の賞賛
返信
1 返信

614件の閲覧回数
miduo
NXP Employee
NXP Employee

Hi,

Attached is the ethernet test code we used for M54455EVB. Hope it is heplful to you.

0 件の賞賛
返信