CodeWarrior Debug issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CodeWarrior Debug issue

743 次查看
muhibraza
Contributor I

Hi all,

I am trying to debug an application for ColdFire MCF52233 Microcontroller using CodeWarrior v6.3 IDE. I have connected a PE Micro Cyclone MAX with USB port with my PC and its turned on. And I am doing all this stuff in a Windows XP 32-bit installation on an Oracle VM VirtualBox. So what happens is that after compiling the project, when I click on Debug>>Connect, an error always pops up saying

"PEMicroProtocolPlugin : No Parallel connection found".

How do I resolve this issue? Attaching a screenshot

标签 (1)
0 项奖励
1 回复

598 次查看
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Muhib Raza,

Which connection did you chose as default when you created the project?

pastedImage_2.png

Please make sure that in you connection settings you have the correct interface selected.


Hope it helps!

Best Regards,
Carlos Mendoza
Technical Support Engineer

0 项奖励