Hello
According to the ANSI C standard CodeWarrior Compiler is generating a warning message when you are calling a function and there is no prototype defined for it.
This is a requirement from the C standard.
Note that you can ask the compiler to generate an error message instead of a warning in that case.
If you are building from the IDE, Check the "Require Function Prototypes" box in the "C/C++ Compiler" Panel.
If you are building from the command line add option -r to your compiler command line
I hope that helps.
CrasyCat