DSP56801 - trouleshoot in CodeWarrior 5.6.1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DSP56801 - trouleshoot in CodeWarrior 5.6.1

2,470 Views
igorman
Contributor I
Hi!
When I debugging DSP56801 in CodeWarrior 5.6.1 I can't  write  any  date  in  petipheral  register. In "Wiev memory"  window  after  execution  comand  ( bfset  #01,  X:0x0fa0)  I dont see 01.
Debuger is set  in  simulator 56801.  Please  help me.

--
Alban Edit: FSL Part Number must figure in Message Subject line.



Message Edited by Alban on 2007-07-30 10:43 AM
Labels (1)
Tags (1)
0 Kudos
5 Replies

338 Views
trytohelp
NXP Employee
NXP Employee
Hi,
 
You meet problem to debug your 56801 application.
Do you meet the problem only in simulator mode or with the hardware too ?
What is the tool version used ?

To do that you must:
- Start the IDE and click on Help | About Metrowerks CodeWarrior.
- Click on Installed Products
- Provide us all info displayed.
- Or you can save them in a txt file.

Be aware the CodeWarrior Development Studio for Freescale 56800/E Digital Signal Controllers Version 8.1.1 is available.This is a patch for the DSC8.0 (must be installed in first)
You can download this version on our web site via the link:
http://www.freescale.com/webapp/sps/site/overview.jsp?nodeId=01272600617882140B

You can have several versions installed on the same PC.
There is only one restriction: install them on separate folder.

Regards
Pascal

 

0 Kudos

338 Views
igorman
Contributor I
Hi!
I just starded work with DSP56801, and only simulating it. 
I done steps, you recomended to recognize version Code Warrior.
My version is Code Warrior Development Studio for DSC56800/E version 8.0.
When I simulated examples, I also did not see any data in perypheral registers.
Thanks for help.
 
Message Edited by t.dowe on 2009-10-15 05:34 PM
0 Kudos

338 Views
trytohelp
NXP Employee
NXP Employee
Hi,
 
Thanks for the details.
Can you please provide me the example showing the problem ?
 
Regards
Pascal
0 Kudos

338 Views
igorman
Contributor I
Hi!
The problem is next.
During debuging in step mode after compleeting
        bfset #01, X:0x0FA0
I see View>Registers>Clock Generation on register PLLCR, that have address X:0x0FA0 and it value is 0x0000. I dont understand why it value is not 0x0001. The debuger is set on 56800 Simulator and processor DSP56F801.
 
Thanks. 
0 Kudos

338 Views
trytohelp
NXP Employee
NXP Employee
Hi,
 
I performed some tests with the simulator and real board on DSP56F803 (not have a 801).
I reproduced the behaviour with the simulator but not on the board.
This seems to be a limitation or a problem with the simulator.
Can I propose you to report this issue on the Suppor team using the web interface ?
By this way I could log this issue in our system (bug tracking).
 

For Technical Support Issues please use Freescale on line support web page.
- Go to following URL: http://www.freescale.com/TechSupport

- Click on Submit a Service Request. You will come to a login page.
- You can submit your request through the web from there.

Thanks
Pascal

0 Kudos