MCUXpresso IDE v11.1.0 - Board SDK Creator

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCUXpresso IDE v11.1.0 - Board SDK Creator

lpcxpresso_supp
NXP Employee
NXP Employee
1 0 1,942

NXP provides MCUXpresso SDKs that are configured for use with our standard evaluation boards. These can be used when carrying out your initial evaluation of our MCUs and early development work. However, in most cases you will reach the point of having your own development or production board. This will mean modifying the pins, clocks and other configuration settings from the evaluation board originally used, generally using the MCUXpresso Config Tools, to match your own board. This will initially be done on a per-project basis.

 

The Board SDK Creator functionality inside MCUXpresso IDE v11.1.0 and later provides a means of generating a secondary SDK to contain these configuration settings for your board, that can be used in conjunction with the original SDK. This can then be used in assisting with the creation of new projects directly for your board and also be easily shared with other members of your team or customers.

 

Using Board SDK Creator

Starting from another SDK, you must first create a new project and adapt it for your own board (with updated pins/clock settings), making any board related changes by adding/modifying files in the project’s board folder. Once the changes are completed, in order to create a board SDK, select File -> New Project… from MCUXpresso IDE’s menu bar and select Board SDK Wizard under MCUXpresso IDE Addons category.

 

pastedImage_3.png

 

The wizard is also available in the right-click menu in the project explorer.

pastedImage_1.png

 

Once started the following dialog will be shown.

pastedImage_3.png

 

The base project will be automatically set if it was already selected in the Project Explorer view. The user interface allows you to define a few basic characteristics of the new SDK being created, such as the name of the custom board, an image of the board, and both brief and more detailed descriptions.

 

pastedImage_5.png

 

If the code requires new C/C++ preprocessor definitions, you can add them using the Defines section

 

Once everything is completed you can choose one of two options under the Wizard target section. The first option asks for a name and location for the SDK zip file.  The second option will open the newly created SDK as a project into the current workspace in MCUXpresso IDE, allowing for more advanced customizations of the SDK.

 

Using the board SDK

 After selecting first option and pressing “Finish” button, the SDK will be automatically imported into the IDE and a zip file for it will be generated. In order to install it on other computers, simply drag & drop the newly created SDK over the “Installed SDKs” view. Note: original SDK (the one used to create the custom SDK) must have been installed first (the image below shows this, with a custom SDK built from the Kinetis K64F Tower Board SDK.)

 

pastedImage_8.png

 

Once installed you can create a new project using the new SDK. The new SDK will appear in the SDK Wizard dialog, as seen for standard SDKs from NXP (see example below).

 

pastedImage_1.png

 

From the SDK Wizard select the new board, making sure to select the new SDK in the “SDKs for Selected MCU” section (bottom right corner of the window). Choose “Next” and “Finish” to close the wizard and close the project. The project will contain all the changes you have made in order to support your custom board.

 

Happy customizing!