FS8530 当WAKE1为低,WAKE2为高时,停止喂狗,FS85复位失败

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FS8530 当WAKE1为低,WAKE2为高时,停止喂狗,FS85复位失败

Jump to solution
2,823 Views
wangchuang
Contributor II

芯片:FS8530

喂狗方式: Challenger Watchdog

现象描述:当WAKE1为低,WAKE2为高的情况下,如果此时仅停止喂狗,不做任何其他操作,则FS85复位,电流掉到0,但是却无法重启

请问:

1. 此现象是否正常

2. 如果不正常,如何避免此现象,即我们想在WAKE2为高的情况下,仍然可以复位成功

3. 如果正常,此现象如何解释,发生此现象时,FS85的状态机是如何跳转的

0 Kudos
1 Solution
2,802 Views
guoweisun
NXP TechSupport
NXP TechSupport

芯片已经进入Deep Fail safe 阶段了,两个方法出来

1:wake1拉低再拉高

2:OTP使能Autoretry 4s就出来了,但是这个是在OTP的阶段更改的,所以还是用第一个方法

View solution in original post

0 Kudos
7 Replies
2,811 Views
guoweisun
NXP TechSupport
NXP TechSupport

1:怎么会无法重启呢?WD错误会影响RSTB/FS0B,但是你再重新启动WD无错误的话应该能起来。

guoweisun_3-1676955246002.png

 

guoweisun_2-1676955207789.png

2:你可以试下断电后等待超过8s再次上电

2:

 

 

 

0 Kudos
2,803 Views
guoweisun
NXP TechSupport
NXP TechSupport

芯片已经进入Deep Fail safe 阶段了,两个方法出来

1:wake1拉低再拉高

2:OTP使能Autoretry 4s就出来了,但是这个是在OTP的阶段更改的,所以还是用第一个方法

0 Kudos
1,862 Views
lkx
Contributor I

为什么进入DFS模式了,状态图上没有这个状态转换呀

 

0 Kudos
2,794 Views
wangchuang
Contributor II
1. 您说的第一种退出方式,状态机跳转流程是否是这样的,
首先当前处于DEEP-FS状态,然后wake1拉低,进入STANDBY DEEP-FS状态,然后wake1拉高,进入WAIT FS
& SUPPLY状态,之后便进入了NORMAL_M状态,此时启动成功。
2. 那么我们有一个疑问,按照您所描述的,WD错误导致复位,进入了DEEP-FS,但是我们在测试的过程中,发现当wake1一直为高的情况下,当WD错误导致复位后,并不会出现上电失败的情况,复位是可以成功的,这种现象如何解释呢,或者状态机的跳转流程是啥样的
3. 目前我们遇到的问题,是我们的程序会概率性启动失败,程序卡死,导致的无法正常喂狗,FS85复位,但是这种情况下,我们的wake2是有可能一直为高的,因此导致板子启动不了,电流一直为0,这种情况下的话,是否可以借助FS85的某些配置来解决呢
0 Kudos
2,785 Views
guoweisun
NXP TechSupport
NXP TechSupport

1. 您说的第一种退出方式,状态机跳转流程是否是这样的, 首先当前处于DEEP-FS状态,然后wake1拉低,进入STANDBY DEEP-FS状态,然后wake1拉高,进入WAIT FS & SUPPLY状态,之后便进入了NORMAL_M状态,此时启动成功。

[gw]对的

2. 那么我们有一个疑问,按照您所描述的,WD错误导致复位,进入了DEEP-FS,但是我们在测试的过程中,发现当wake1一直为高的情况下,当WD错误导致复位后,并不会出现上电失败的情况,复位是可以成功的,这种现象如何解释呢,或者状态机的跳转流程是啥样的

【gw】就是OTP_Autoretry在OTP的阶段被enable 了所以不改变WAKE1也会自动跳转到standbydeep_fs这个阶段但是你看他需要等4s.

Exit of DEEP-FS mode is only possible by WAKE1 = 0 or after 4 s if the autoretry feature
is activated by OTP_Autorety_en bit. The number of autroretry can be limited to 15 or
infinite depending on OTP_Autoretry_infinite bit. VPRE restarts when VSUP > VSUP_UVH
and WAKE1 > WAKE12VIH.

guoweisun_0-1676978709871.png

 

0 Kudos
2,807 Views
wangchuang
Contributor II
是的,WD错误导致了复位,正常情况下应该是下电,电流降为0,在上电,电流回升。
1. 但是目前的情况是,在WAKE2为高的情况下,发生了复位的话,下电,电流降为了0,然后就一直持续在0了,电流并没有回升。
2. 在1中的情况下,如果WAKE2为低了,然后WAKE1或者WAKE2中的任意一个为高,则又是可以上电成功了的
0 Kudos
1,860 Views
lkx
Contributor I
老兄, 解决这个问题了嘛
0 Kudos