IMX6ULL- Wifi/BT modules supported

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6ULL- Wifi/BT modules supported

1,214 Views
Raghavan
NXP Employee
NXP Employee

Hello Support

Can you please advise which WIFI-BT module is tested and proven with IMX6ULL and Linux BSP

Regards

Raghavan

0 Kudos
2 Replies

673 Views
jerseyyang
Contributor III

i am developing the WIFI function in IMX6UL with the MuRata 1DX WIFI module (BCM4343W) 

linux BSP 3.14.52

0 Kudos

673 Views
igorpadykov
NXP Employee
NXP Employee

Hi Raghavan

it is BCM4339 according to Table 9. Supported features attached Release Notes

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos