<Service 'recovery' killed by signal 11> when using 800x480px screen on Android 6.0.1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

<Service 'recovery' killed by signal 11> when using 800x480px screen on Android 6.0.1

Jump to solution
1,861 Views
tootzoe
Contributor III

Hi  all , 

  i encountered a  bug,  i working on android 6.0.1 kernel 4.1.15, i using a screen with 800x400 pixel resolution, everythin works well excepting on recovery mode.

  i make my board into recovery mode with ota update,  update process goes normally initially , when it going to be done, an error says "Service 'recovery' killed by signal 11" occurred  , then board did not reboot, and recovery progress clean 0 , then restart recovery progress.

when i change the resolution of screen back to 1024x768px, the ota recovery work well, so i thought the reason is that recovery program didn't find correct  image resource (png image) under 800x480px mode, this lead to a null pointer reference when finishing the recovery progress, i can't identify which png file now,

if somebody tell me how to fix this issues would be great appreciate! 

best regards!

 toot_hzf

Labels (1)
0 Kudos
1 Solution
909 Views
tootzoe
Contributor III

eventually i find the bug was on coping log file action, in recovery.cpp line  396 ,

   // copy_logs();

 i comment this line, and ota upgrade OK now.......

By the way , debugging recovery section is time exhaust.... 

View solution in original post

0 Kudos
2 Replies
910 Views
tootzoe
Contributor III

eventually i find the bug was on coping log file action, in recovery.cpp line  396 ,

   // copy_logs();

 i comment this line, and ota upgrade OK now.......

By the way , debugging recovery section is time exhaust.... 

0 Kudos
909 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Huang Zhanfei,

I’m glad you found the issue. Thanks for sharing the fix! I’m sure it will help another community users and save a lot of debugging time! Debugging is always time consuming, it certainly is in Android in general.

Regards,

0 Kudos