Dead coincell and tamper detection

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Dead coincell and tamper detection

628 Views
adriengravouill
Contributor I

Hi community,  

I'm developing a custom board with the IMX6SL processor, based on EDK.

I will use integrated RTC and tamper detection, which both required an external coincell. I need some help to choose the coincell correctly. My system will run only when it is supplied from a wall USB adapter, so no other battery available.

  1. It seems that's when system is off, it drains up to 250µA from the coincell, which is huge.  A standard rechargeable CR2032 capacity is 40mAh. So, the RTC can work 6 day before being out of power. After that, I will need to plug the board to my wall adapter to make the board working again : is the low voltage of the coincell a problem?
  2. PF0100 integrates a Lithium charger, which current charging is 60µA, so it will take something like 27 days to charge the RTC's coincell?
  3. Finally, is the first case, when battery will be out of power, what will happen with tamper detection when I will bring back the power?

Best regards,

Labels (2)
0 Kudos
3 Replies

488 Views
igorpadykov
NXP Employee
NXP Employee

1. this is max. value, typical 41uA as gives Table 12 i.MX6SL Datasheet

http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6SLCEC.pdf

Low voltage of the coincell (below values in Table 9. Operating Ranges)

may not guarantee proper SNVS block operaton (time, tamper functions)

2. right

3. >when battery will be out of power, what will happen with tamper detection when I will bring back the power?

Fully powered processor will work fine according to its specifcations.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

488 Views
adriengravouill
Contributor I

Thank you for your answer.

When a low voltage of the coincell condition occurs, Is SNVS block can generate a false tamper detection?

In that case, it will result with an "Activation of the security related hardware (e.g. automatic and immediate erasure of the
Zeroizable Master Key and deny access and erasure of secure memory contents)", so at next start'up software will be bricked?

How to deal with this kind of problem?

0 Kudos

488 Views
igorpadykov
NXP Employee
NXP Employee

Low voltage of the coincell (below values in Table 9. Operating Ranges)

may not guarantee proper SNVS block operaton.

0 Kudos