Hello,
We are interfacing Atmel MXT224E touchscreen with imx6DL Processor in Android Kitkat 4.4.2.
We have connected it to I2C-2 and interrupt pin is used in GPIO_1_8.
We are getting acknowledge from Touchscreen with Family ID, Variant ID and version correctly.
But some problem is with interrupt. When we touch the screen interrupt number is not incremented after checking using
cat /proc/interrupts command but if manually short it to Ground then it will increment the number.
For this problem any configuration setting we have to do in kernel setting?
Hello,
I am facing a problem with interrupts. When I give the command "cat /proc/interrupts" I can see atmel_mxt_ts interrupt but when I touch the screen it is not responding that is I cannot see the interrupt requests increasing when pressing the touchscreen. Can anyone help with this? Does anybody have the documentation for configuring the interrupts in the board file or do I have to make changes in driver file? Thanks in advance.
Hello,
I am facing a problem with interrupts. When I give the command "cat /proc/interrupts" I can see atmel_mxt_ts interrupt but when I touch the screen it is not responding that is I cannot see the interrupt requests increasing when pressing the touchscreen. Can anyone help with this? Does anybody have the documentation for configuring the interrupts in the board file or do I have to make changes in driver file? Thanks in advance.
Hi VIVEK
interrupt could be triggered by level or edge, which can be configured,
for android interrupt handling example one can look at
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------