iMX6 kernel 3.10.53 crash

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6 kernel 3.10.53 crash

759 Views
awadheshmaurya
Contributor I

Hi,

I am using kernel 3.10.53 and Debian Jessie. I am using it for 10 month it was working fine. But from some days I am error looks like kernel panic as follow:

[  360.786416] systemd[1]: Started Session c3 of user root.

[  907.452372] systemd[1]: Starting Cleanup of Temporary Directories...

[  907.602903] systemd[1]: Started Cleanup of Temporary Directories.

[ 1656.347129] xhci_hcd 0000:01:00.0: ERROR Transfer event TRB DMA ptr not part                                                                                         of current TD

[ 1661.355636] xhci_hcd 0000:01:00.0: ERROR Transfer event TRB DMA ptr not part                                                                                         of current TD

[ 1666.364228] xhci_hcd 0000:01:00.0: ERROR Transfer event TRB DMA ptr not part                                                                                         of current TD

[ 1671.372823] xhci_hcd 0000:01:00.0: ERROR Transfer event TRB DMA ptr not part                                                                                         of current TD

[ 1676.381289] xhci_hcd 0000:01:00.0: ERROR Transfer event TRB DMA ptr not part                                                                                         of current TD

[ 1681.390003] xhci_hcd 0000:01:00.0: ERROR Transfer event TRB DMA ptr not part                                                                                         of current TD

[ 1686.398744] xhci_hcd 0000:01:00.0: ERROR Transfer event TRB DMA ptr not part                                                                                         of current TD

[ 1691.407449] xhci_hcd 0000:01:00.0: ERROR Transfer event TRB DMA ptr not part                                                                                         of current TD

[ 1696.415941] xhci_hcd 0000:01:00.0: ERROR Transfer event TRB DMA ptr not part                                                                                         of current TD

[ 1701.424788] xhci_hcd 0000:01:00.0: ERROR Transfer event TRB DMA ptr not part                                                                                         of current TD

[ 1706.433439] xhci_hcd 0000:01:00.0: ERROR Transfer event TRB DMA ptr not part                                                                                         of current TD

[ 1711.441990] xhci_hcd 0000:01:00.0: ERROR Transfer event TRB DMA ptr not part                                                                                         of current TD

[ 1716.450872] xhci_hcd 0000:01:00.0: ERROR Transfer event TRB DMA ptr not part                                                                                         of current TD

[ 1721.459758] xhci_hcd 0000:01:00.0: ERROR Transfer event TRB DMA ptr not part                                                                                         of current TD

[ 1726.468372] xhci_hcd 0000:01:00.0: ERROR Transfer event TRB DMA ptr not part                                                                                         of current TD

[ 1731.477003] xhci_hcd 0000:01:00.0: ERROR Transfer event TRB DMA ptr not part                                                                                         of current TD

[ 1736.486992] xhci_hcd 0000:01:00.0: ERROR Transfer event TRB DMA ptr not part                                                                                         of current TD

[ 1741.495618] xhci_hcd 0000:01:00.0: ERROR Transfer event TRB DMA ptr not part                                                                                         of current TD

[ 1746.504312] xhci_hcd 0000:01:00.0: ERROR Transfer event TRB DMA ptr not part                                                                                         of current TD

[ 1751.512831] xhci_hcd 0000:01:00.0: ERROR Transfer event TRB DMA ptr not part                                                                                         of current TD

[ 1756.521310] xhci_hcd 0000:01:00.0: ERROR Transfer event TRB DMA ptr not part                                                                                         of current TD

[ 1761.529807] xhci_hcd 0000:01:00.0: ERROR Transfer event TRB DMA ptr not part                                                                                         of current TD

[ 1766.538489] xhci_hcd 0000:01:00.0: ERROR Transfer event TRB DMA ptr not part                                                                                         of current TD

[ 1771.547119] xhci_hcd 0000:01:00.0: ERROR Transfer event TRB DMA ptr not part                                                                                         of current TD

[ 1776.555697] xhci_hcd 0000:01:00.0: ERROR Transfer event TRB DMA ptr not part                                                                                         of current TD

[ 1781.564316] xhci_hcd 0000:01:00.0: ERROR Transfer event TRB DMA ptr not part                                                                                         of current TD

[ 1786.573119] xhci_hcd 0000:01:00.0: ERROR Transfer event TRB DMA ptr not part                                                                                         of current TD

[ 1791.581749] xhci_hcd 0000:01:00.0: ERROR Transfer event TRB DMA ptr not part                                                                                         of current TD

[ 1796.590265] xhci_hcd 0000:01:00.0: ERROR Transfer event TRB DMA ptr not part                                                                                         of current TD

[ 1801.598753] xhci_hcd 0000:01:00.0: ERROR Transfer event TRB DMA ptr not part                                                                                         of current TD

[ 1806.607373] xhci_hcd 0000:01:00.0: ERROR Transfer event TRB DMA ptr not part                                                                                         of current TD

[ 1811.615997] xhci_hcd 0000:01:00.0: ERROR Transfer event TRB DMA ptr not part                                                                                         of current TD

[ 1816.624602] xhci_hcd 0000:01:00.0: ERROR Transfer event TRB DMA ptr not part                                                                                         of current TD

[ 1821.633235] xhci_hcd 0000:01:00.0: ERROR Transfer event TRB DMA ptr not part                                                                                         of current TD

[ 1826.641921] xhci_hcd 0000:01:00.0: ERROR Transfer event TRB DMA ptr not part                                                                                         of current TD

[ 1831.650645] xhci_hcd 0000:01:00.0: ERROR Transfer event TRB DMA ptr not part                                                                                         of current TD

[ 1836.659240] xhci_hcd 0000:01:00.0: ERROR Transfer event TRB DMA ptr not part                                                                                         of current TD

[ 1841.667786] xhci_hcd 0000:01:00.0: ERROR Transfer event TRB DMA ptr not part                                                                                         of current TD

[ 1846.677532] xhci_hcd 0000:01:00.0: ERROR Transfer event TRB DMA ptr not part                                                                                         of current TD

[ 1851.686186] xhci_hcd 0000:01:00.0: ERROR Transfer event TRB DMA ptr not part                                                                                         of current TD

[ 1856.694811] xhci_hcd 0000:01:00.0: ERROR Transfer event TRB DMA ptr not part                                                                                         of current TD

[ 1861.162446] xhci_hcd 0000:01:00.0: ERROR Transfer event TRB DMA ptr not part                                                                                         of current TD

[ 1861.703366] xhci_hcd 0000:01:00.0: ERROR Transfer event TRB DMA ptr not part                                                                                         of current TD

[ 1861.954461] xhci_hcd 0000:01:00.0: ERROR Transfer event TRB DMA ptr not part                                                                                         of current TD

[ 1862.012817] Unable to handle kernel NULL pointer dereference at virtual addre                                                                                        ss 000000dd

[ 1862.021046] pgd = d8e58000

[ 1862.023804] [000000dd] *pgd=68cae831, *pte=00000000, *ppte=00000000

[ 1862.030130] Internal error: Oops: 17 [#1] PREEMPT SMP ARM

[ 1862.035533] Modules linked in: smsc95xx usbnet wlcore_sdio mxc_dcic

[ 1862.041889] CPU: 0 PID: 1027 Comm: Fieldbus Not tainted 3.10.53-ge55b1ce #13

[ 1862.048944] task: d8692400 ti: d8fce000 task.ti: d8fce000

[ 1862.054363] PC is at __kmalloc+0x7c/0x1d8

[ 1862.058379] LR is at __kmalloc+0x60/0x1d8

[ 1862.062395] pc : [<800cf5a8>]    lr : [<800cf58c>]    psr: 20070013

[ 1862.062395] sp : d8fcfd10  ip : 7f00c7a8  fp : d84844c0

[ 1862.073876] r10: 000000a1  r9 : 04ddefa0  r8 : d8fce000

[ 1862.079105] r7 : 000000d0  r6 : 010e6000  r5 : 000000dd  r4 : d8001f00

[ 1862.085637] r3 : 00000000  r2 : 00000001  r1 : 000000d0  r0 : 00000000

[ 1862.092174] Flags: nzCv  IRQs on  FIQs on  Mode SVC_32  ISA ARM  Segment user

[ 1862.099313] Control: 10c53c7d  Table: 68e5804a  DAC: 00000015

[ 1862.105064] Process Fieldbus (pid: 1027, stack limit = 0xd8fce238)

[ 1862.111247] Stack: (0xd8fcfd10 to 0xd8fd0000)

[ 1862.115611] fd00:                                     00000004 00000004 00000                                                                                        114 d8fcfdb4

[ 1862.123796] fd20: 00000000 000000c0 000000a1 7f00c720 60070013 000000c0 7519c                                                                                        dc4 80689494

[ 1862.131981] fd40: 00000000 80355e84 00000000 d84844c0 00000004 00000114 00000                                                                                        000 000000c0

[ 1862.140165] fd60: 000000a1 00000000 7519cdc4 7f00c7fc 00000114 d8fcfdb4 00000                                                                                        004 00000118

[ 1862.148353] fd80: 00000000 00000114 d8fcfdd4 00000000 d84844c0 0002628c 00000                                                                                        001 7f01429c

[ 1862.156537] fda0: 00000114 d8fcfdb4 00000004 81e19b80 00001a6d 00000000 00001                                                                                        a6d 80d380c0

[ 1862.164721] fdc0: d84844c0 00000000 d84844c0 7f01441c d8484000 d8484000 d8484                                                                                        000 d8484550

[ 1862.172906] fde0: 00000000 d84844c0 d84844e0 7f01451c 80d33b80 81e19bc8 d8fcf                                                                                        e70 d8484550

[ 1862.181090] fe00: d8484000 d8484000 00000001 d8fce008 d6a96c20 803dd9b4 7f014                                                                                        5f4 d8484000

[ 1862.189274] fe20: d8fcfe70 d8484000 d8fcfed0 00000000 d8fce008 80599910 00000                                                                                        000 7519cd98

[ 1862.197458] fe40: 00000001 8059ae5c 60004008 00000000 80d41bc8 80d33b80 d8fcf                                                                                        efc 00000001

[ 1862.205641] fe60: 000001b1 81e18660 81e18628 87ee3fc5 00000001 000002cf 00000                                                                                        280 02000000

[ 1862.213825] fe80: 01000001 00000000 00000000 00000000 00000000 00000000 00000                                                                                        000 d8fce000

[ 1862.222010] fea0: 81e1c300 00008946 80d872c0 7519cdc4 d8fcfed0 00000000 00000                                                                                        000 d6a96c20

[ 1862.230194] fec0: 7519cdc4 805a97cc d8fce008 80150015 31687465 00000000 00000                                                                                        000 00000000

[ 1862.238379] fee0: 7519cd98 76fc9c08 00000001 00000000 00008946 00008946 d9158                                                                                        e40 00000001

[ 1862.246563] ff00: 7519cdc4 d9158e40 d8fce000 d6a96c20 7519cdc4 800ead6c d87eb                                                                                        300 80d4e500

[ 1862.254747] ff20: 80aa28c0 800dc924 00000020 800ed1e0 80d3f2d0 d8fcff58 00000                                                                                        003 800dca3c

[ 1862.262931] ff40: 00000020 80d3f2d0 d6a96c00 00000000 d6a96c00 80581400 7ebf8                                                                                        c90 806891f8

[ 1862.271115] ff60: d8ca9200 00008946 00000008 00000001 7519cdc4 d9158e40 d8fce                                                                                        000 00000000

[ 1862.279300] ff80: 7ebf8c90 800eaf6c 7519cdf0 00000001 0006ed38 7519d450 7519d                                                                                        450 00000036

[ 1862.287484] ffa0: 8000e204 8000e080 0006ed38 7519d450 00000008 00008946 7519c                                                                                        dc4 7519cdc4

[ 1862.295668] ffc0: 0006ed38 7519d450 7519d450 00000036 7519cf90 00000000 7519d                                                                                        684 7ebf8c90

[ 1862.303853] ffe0: 0006edf8 7519cd8c 0001af03 7618b036 20070030 00000008 00000                                                                                        000 00000000

[ 1862.312059] [<800cf5a8>] (__kmalloc+0x7c/0x1d8) from [<7f00c720>] (__usbnet_r                                                                                        ead_cmd.isra.24+0x38/0xc0 [usbnet])

[ 1862.322257] [<7f00c720>] (__usbnet_read_cmd.isra.24+0x38/0xc0 [usbnet]) from                                                                                         [<7f00c7fc>] (usbnet_read_cmd+0x54/0x74 [usbnet])

[ 1862.333666] [<7f00c7fc>] (usbnet_read_cmd+0x54/0x74 [usbnet]) from [<7f01429c                                                                                        >] (__smsc95xx_read_reg+0x54/0x90 [smsc95xx])

[ 1862.344726] [<7f01429c>] (__smsc95xx_read_reg+0x54/0x90 [smsc95xx]) from [<7f                                                                                        01441c>] (__smsc95xx_phy_wait_not_busy+0x54/0x90 [smsc95xx])

[ 1862.357085] [<7f01441c>] (__smsc95xx_phy_wait_not_busy+0x54/0x90 [smsc95xx])                                                                                         from [<7f01451c>] (__smsc95xx_mdio_read+0x34/0x10c [smsc95xx])

[ 1862.369626] [<7f01451c>] (__smsc95xx_mdio_read+0x34/0x10c [smsc95xx]) from [<                                                                                        803dd9b4>] (mii_ethtool_gset+0x64/0x214)

[ 1862.380253] [<803dd9b4>] (mii_ethtool_gset+0x64/0x214) from [<80599910>] (__e                                                                                        thtool_get_settings+0x50/0x7c)

[ 1862.390009] [<80599910>] (__ethtool_get_settings+0x50/0x7c) from [<8059ae5c>]                                                                                         (dev_ethtool+0x3b0/0x1fcc)

[ 1862.399504] [<8059ae5c>] (dev_ethtool+0x3b0/0x1fcc) from [<805a97cc>] (dev_io                                                                                        ctl+0x458/0x80c)

[ 1862.408042] [<805a97cc>] (dev_ioctl+0x458/0x80c) from [<800ead6c>] (do_vfs_io                                                                                        ctl+0x400/0x5c8)

[ 1862.416577] [<800ead6c>] (do_vfs_ioctl+0x400/0x5c8) from [<800eaf6c>] (SyS_io                                                                                        ctl+0x38/0x64)

[ 1862.424947] [<800eaf6c>] (SyS_ioctl+0x38/0x64) from [<8000e080>] (ret_fast_sy                                                                                        scall+0x0/0x30)

[ 1862.433394] Code: e7965005 e3550000 0a00001f e5943014 (e795c003)

[ 1862.440417] ---[ end trace 2a826d12562d797f ]---

[ 1862.447812] Unable to handle kernel NULL pointer dereference at virtual addre                                                                                        ss 000000dd

[ 1862.456225] pgd = d8ca0000

[ 1862.459027] Unable to handle kernel NULL pointer dereference at virtual addre                                                                                        ss 000000dd

[ 1862.467188] pgd = d8e48000

[ 1862.467384] [000000dd] *pgd=688cd831, *pte=00000000, *ppte=00000000

[ 1862.467393] Internal error: Oops: 17 [#2] PREEMPT SMP ARM

[ 1862.467404] Modules linked in: smsc95xx usbnet wlcore_sdio mxc_dcic

[ 1862.467412] CPU: 2 PID: 1001 Comm: CM Tainted: G      D      3.10.53-ge55b1ce                                                                                         #13

[ 1862.467416] task: d8895c00 ti: d8aca000 task.ti: d8aca000

[ 1862.467433] PC is at __kmalloc+0x7c/0x1d8

[ 1862.467438] LR is at __kmalloc+0x60/0x1d8

[ 1862.467444] pc : [<800cf5a8>]    lr : [<800cf58c>]    psr: 200f0013

[ 1862.467444] sp : d8acbef8  ip : d8aca008  fp : 00000000

[ 1862.467447] r10: 00000004  r9 : 04ddf038  r8 : d8aca000

[ 1862.467451] r7 : 000000d0  r6 : 010e6000  r5 : 000000dd  r4 : d8001f00

[ 1862.467455] r3 : 00000000  r2 : 00000001  r1 : 000000d0  r0 : 00000000

[ 1862.467460] Flags: nzCv  IRQs on  FIQs on  Mode SVC_32  ISA ARM  Segment user

[ 1862.467463] Control: 10c53c7d  Table: 68ca004a  DAC: 00000015

[ 1862.467467] Process CM (pid: 1001, stack limit = 0xd8aca238)

[ 1862.467471] Stack: (0xd8acbef8 to 0xd8acc000)

[ 1862.467475] bee0:                                                       000d0                                                                                        019 d8aca000

[ 1862.467482] bf00: 00000004 0003df44 30402005 d8aca000 00000004 80238a5c 80d51                                                                                        f9c 80291e8c

[ 1862.467488] bf20: 80d51fa0 000d0019 d8aca000 00000004 80d51f58 30402005 d8aca                                                                                        000 00000000

[ 1862.467494] bf40: 00000000 802396f8 80d51fa4 d8aca008 80d51f58 80d51f9c 80d51                                                                                        f58 000003b6

[ 1862.467500] bf60: 00000001 00000000 761ed000 00000004 000d0019 000000d8 00000                                                                                        12d 8000e204

[ 1862.467506] bf80: d8aca000 00000000 00000000 80239a98 00000800 00004000 00000                                                                                        3b6 00000000

[ 1862.467512] bfa0: 761ed000 8000e080 00000000 761ed000 000d0019 0003df40 00000                                                                                        004 00000800

[ 1862.467518] bfc0: 00000000 761ed000 000000d8 0000012d 00000000 00000000 76fdb                                                                                        000 00000000

[ 1862.467526] bfe0: 00000000 7ea74c50 7619742b 76197432 800f0030 000d0019 7f75e                                                                                        821 7f75ec21

[ 1862.467545] [<800cf5a8>] (__kmalloc+0x7c/0x1d8) from [<80238a5c>] (load_msg+0                                                                                        x28/0x18c)

[ 1862.467556] [<80238a5c>] (load_msg+0x28/0x18c) from [<802396f8>] (do_msgsnd+0                                                                                        x58/0x3a8)

[ 1862.467565] [<802396f8>] (do_msgsnd+0x58/0x3a8) from [<80239a98>] (SyS_msgsnd                                                                                        +0x50/0x60)

[ 1862.467580] [<80239a98>] (SyS_msgsnd+0x50/0x60) from [<8000e080>] (ret_fast_s                                                                                        yscall+0x0/0x30)

[ 1862.467588] Code: e7965005 e3550000 0a00001f e5943014 (e795c003)

[ 1862.467593] ---[ end trace 2a826d12562d7980 ]---

[ 1862.679014] [000000dd] *pgd=688ea831, *pte=00000000, *ppte=00000000

[ 1862.685376] Internal error: Oops: 17 [#3] PREEMPT SMP ARM

[ 1862.690780] Modules linked in: smsc95xx usbnet wlcore_sdio mxc_dcic

[ 1862.697132] CPU: 0 PID: 1039 Comm: PC Tainted: G      D      3.10.53-ge55b1ce                                                                                         #13

[ 1862.704618] task: d8e00400 ti: d9022000 task.ti: d9022000

[ 1862.710031] PC is at __kmalloc+0x7c/0x1d8

[ 1862.714046] LR is at __kmalloc+0x60/0x1d8

[ 1862.718061] pc : [<800cf5a8>]    lr : [<800cf58c>]    psr: 200f0013

[ 1862.718061] sp : d9023ef8  ip : d9022008  fp : 7ea17bd8

[ 1862.729541] r10: 00000004  r9 : 04ddf048  r8 : d9022000

[ 1862.734767] r7 : 000000d0  r6 : 010e6000  r5 : 000000dd  r4 : d8001f00

[ 1862.741296] r3 : 00000000  r2 : 00000001  r1 : 000000d0  r0 : 00000000

[ 1862.747828] Flags: nzCv  IRQs on  FIQs on  Mode SVC_32  ISA ARM  Segment user

[ 1862.754965] Control: 10c53c7d  Table: 68e4804a  DAC: 00000015

[ 1862.760712] Process PC (pid: 1039, stack limit = 0xd9022238)

[ 1862.766374] Stack: (0xd9023ef8 to 0xd9024000)

[ 1862.770734] 3ee0:                                                       000f0                                                                                        01c d9022000

[ 1862.778916] 3f00: 00000004 7582be24 2023200e d9022000 00000004 80238a5c 00000                                                                                        000 80238a10

[ 1862.787099] 3f20: 80239408 000f001c d9022000 00000004 80d51f58 2023200e d9022                                                                                        000 00000000

[ 1862.795280] 3f40: 7ea17bd8 802396f8 00000000 d9022008 80d51f58 00100100 00200                                                                                        200 d8e00400

[ 1862.803461] 3f60: 00000001 00000000 00000004 00000004 000f001c 7582c450 00000                                                                                        12d 8000e204

[ 1862.811642] 3f80: d9022000 00000000 7ea17bd8 80239a98 00000000 80239e88 00000                                                                                        000 00000000

[ 1862.819823] 3fa0: 7582c450 8000e080 00000000 7582c450 000f001c 7582be20 00000                                                                                        004 00000000

[ 1862.828005] 3fc0: 00000000 7582c450 7582c450 0000012d 7582bf90 00000000 7582c                                                                                        684 7ea17bd8

[ 1862.836187] 3fe0: 00000000 7582bdd8 7610142b 76101432 800f0030 000f001c 00000                                                                                        000 00000000

[ 1862.844383] [<800cf5a8>] (__kmalloc+0x7c/0x1d8) from [<80238a5c>] (load_msg+0                                                                                        x28/0x18c)

[ 1862.852397] [<80238a5c>] (load_msg+0x28/0x18c) from [<802396f8>] (do_msgsnd+0                                                                                        x58/0x3a8)

[ 1862.860407] [<802396f8>] (do_msgsnd+0x58/0x3a8) from [<80239a98>] (SyS_msgsnd                                                                                        +0x50/0x60)

[ 1862.868512] [<80239a98>] (SyS_msgsnd+0x50/0x60) from [<8000e080>] (ret_fast_s                                                                                        yscall+0x0/0x30)

[ 1862.877042] Code: e7965005 e3550000 0a00001f e5943014 (e795c003)

[ 1862.883210] ---[ end trace 2a826d12562d7981 ]---

[ 1862.893365] Unable to handle kernel NULL pointer dereference at virtual addre                                                                                        ss 000000dd

[ 1862.901489] pgd = d8e54000

[ 1862.904217] [000000dd] *pgd=68683831, *pte=00000000, *ppte=00000000

[ 1862.910548] Internal error: Oops: 17 [#4] PREEMPT SMP ARM

[ 1862.915950] Modules linked in: smsc95xx usbnet wlcore_sdio mxc_dcic

[ 1862.922305] CPU: 0 PID: 5946 Comm: DIO Tainted: G      D      3.10.53-ge55b1c                                                                                        e #13

[ 1862.929879] task: d800c000 ti: d9630000 task.ti: d9630000

[ 1862.935295] PC is at kmem_cache_alloc+0x68/0x1a8

[ 1862.939920] LR is at kmem_cache_alloc+0x4c/0x1a8

[ 1862.944545] pc : [<800cf76c>]    lr : [<800cf750>]    psr: 200f0013

[ 1862.944545] sp : d9631e48  ip : d8139c38  fp : d8d60600

[ 1862.956025] r10: d8139c68  r9 : 04ddf048  r8 : d9630000

[ 1862.961255] r7 : 000000d0  r6 : 010e6000  r5 : d8001f00  r4 : 000000dd

[ 1862.967786] r3 : 00000000  r2 : 00000001  r1 : 000000d0  r0 : 00000000

[ 1862.974318] Flags: nzCv  IRQs on  FIQs on  Mode SVC_32  ISA ARM  Segment user

[ 1862.981457] Control: 10c53c7d  Table: 68e5404a  DAC: 00000015

[ 1862.987207] Process DIO (pid: 5946, stack limit = 0xd9630238)

[ 1862.992956] Stack: (0xd9631e48 to 0xd9632000)

[ 1862.997322] 1e40:                   d8139c9c 72c00508 00000000 d844e958 d8139                                                                                        c00 80deae88

[ 1863.005507] 1e60: d8139c68 8042f880 81e29bc8 8005cbb8 800101e8 f805a270 00000                                                                                        1b1 d8d60e80

[ 1863.013692] 1e80: 81e19b80 d8d60e80 81e18660 d9630028 ffffffff d8139c38 80d3e                                                                                        7d0 80689494

[ 1863.021875] 1ea0: 00000000 8004e18c 00000000 00000000 d80b401c d83c4000 80d3e                                                                                        7d0 8000e050

[ 1863.030061] 1ec0: 80d615c4 00000002 00000000 00000000 72c004e8 00000018 00000                                                                                        000 00000000

[ 1863.038245] 1ee0: 00000000 00000000 00000000 72c00468 00000000 802c550a d8d3a                                                                                        c00 00000001

[ 1863.046430] 1f00: 72c00508 d8d3ac00 d9630000 d844e958 72c00508 800ead6c 00000                                                                                        000 80116ba4

[ 1863.054614] 1f20: 00000000 80031010 f805a270 000001b1 d9631f38 d9631f70 00000                                                                                        000 00000000

[ 1863.062798] 1f40: 00000000 d9631f50 00000000 00000000 bc6aeb88 000001b1 d8d3b                                                                                        840 00000001

[ 1863.070982] 1f60: 00000000 802c550a 00000011 00000001 72c00508 d8d3ac00 d9630                                                                                        000 00000000

[ 1863.079168] 1f80: 76ee6260 800eaf6c 01986cd0 00000001 00000060 72c00508 72c00                                                                                        468 00000036

[ 1863.087352] 1fa0: 8000e204 8000e080 00000060 72c00508 00000011 802c550a 72c00                                                                                        508 00000018

[ 1863.095536] 1fc0: 00000060 72c00508 72c00468 00000036 00000000 72c004c8 00000                                                                                        001 76ee6260

[ 1863.103723] 1fe0: 76ef10ac 735fec5c 76ee2943 76186036 200f0030 00000011 222c5                                                                                        d7d 666e6f63

[ 1863.111925] [<800cf76c>] (kmem_cache_alloc+0x68/0x1a8) from [<8042f880>] (usb                                                                                        dev_ioctl+0x924/0x1f64)

[ 1863.121075] [<8042f880>] (usbdev_ioctl+0x924/0x1f64) from [<800ead6c>] (do_vf                                                                                        s_ioctl+0x400/0x5c8)

[ 1863.129958] [<800ead6c>] (do_vfs_ioctl+0x400/0x5c8) from [<800eaf6c>] (SyS_io                                                                                        ctl+0x38/0x64)

[ 1863.138329] [<800eaf6c>] (SyS_ioctl+0x38/0x64) from [<8000e080>] (ret_fast_sy                                                                                        scall+0x0/0x30)

[ 1863.146776] Code: e7964004 e3540000 0a00001f e5953014 (e794c003)

[ 1863.158033] ---[ end trace 2a826d12562d7982 ]---

[ 1863.211641] Unable to handle kernel NULL pointer dereference at virtual addre                                                                                        ss 000000dd

[ 1863.219736] pgd = d8e58000

[ 1863.224500] [000000dd] *pgd=68cae831, *pte=00000000, *ppte=00000000

[ 1863.230818] Internal error: Oops: 17 [#5] PREEMPT SMP ARM

[ 1863.236220] Modules linked in: smsc95xx usbnet wlcore_sdio mxc_dcic

[ 1863.242567] CPU: 0 PID: 1030 Comm: Fieldbus Tainted: G      D      3.10.53-ge                                                                                        55b1ce #13

[ 1863.250574] task: d8690400 ti: d8fd4000 task.ti: d8fd4000

[ 1863.255985] PC is at kmem_cache_alloc+0x68/0x1a8

[ 1863.260608] LR is at kmem_cache_alloc+0x4c/0x1a8

[ 1863.265229] pc : [<800cf76c>]    lr : [<800cf750>]    psr: 20070013

[ 1863.265229] sp : d8fd5ec0  ip : 00000000  fp : d948f164

[ 1863.276707] r10: d948f000  r9 : 04ddf048  r8 : d8fd4000

[ 1863.281934] r7 : 000000d0  r6 : 010e6000  r5 : d8001f00  r4 : 000000dd

[ 1863.288464] r3 : 00000000  r2 : 00000001  r1 : 000000d0  r0 : 00000000

[ 1863.294994] Flags: nzCv  IRQs on  FIQs on  Mode SVC_32  ISA ARM  Segment user

[ 1863.302131] Control: 10c53c7d  Table: 68e5804a  DAC: 00000015

[ 1863.307879] Process Fieldbus (pid: 1030, stack limit = 0xd8fd4238)

[ 1863.314062] Stack: (0xd8fd5ec0 to 0xd8fd6000)

[ 1863.318426] 5ec0: 003d0f00 d8fd4028 80d93780 80d48ba8 d8bf00c4 737ff4b8 d948f                                                                                        000 80047588

[ 1863.326607] 5ee0: 80d91f10 737fef88 00000000 8004fd2c 00000000 80d48b50 d9372                                                                                        000 d9373fb0

[ 1863.334790] 5f00: d948f000 003d0f00 d8fd4028 80d93780 80d48ba8 d8bf00c4 737ff                                                                                        4b8 d948f000

[ 1863.342971] 5f20: d948f164 8002bd04 d948f1dc 00000000 737fef88 00000000 00010                                                                                        000 d87ff000

[ 1863.351153] 5f40: d8fd5f6c 00000000 00000000 003d0f00 00020200 00000000 00000                                                                                        000 737ff4b8

[ 1863.359334] 5f60: d8fd4000 00000000 00697c40 8002c3f4 00000000 00000000 737ff                                                                                        4b8 76f28178

[ 1863.367516] 5f80: 00000000 00000078 737ff4b8 76f28178 00000000 00000078 8000e                                                                                        204 d8fd4000

[ 1863.375700] 5fa0: 00000000 8000e080 737ff4b8 76f28178 003d0f00 737fef88 737ff                                                                                        4b8 737ff910

[ 1863.383883] 5fc0: 737ff4b8 76f28178 00000000 00000078 737fef90 737ff450 737ff                                                                                        684 00697c40

[ 1863.392064] 5fe0: 003d0f00 76fa9348 76f0d51d 7618ffe6 20070030 003d0f00 00000                                                                                        000 00000000

[ 1863.400270] [<800cf76c>] (kmem_cache_alloc+0x68/0x1a8) from [<80047588>] (all                                                                                        oc_pid+0x18/0x4ac)

[ 1863.408980] [<80047588>] (alloc_pid+0x18/0x4ac) from [<8002bd04>] (copy_proce                                                                                        ss.part.55+0x85c/0xe8c)

[ 1863.418123] [<8002bd04>] (copy_process.part.55+0x85c/0xe8c) from [<8002c3f4>]                                                                                         (do_fork+0x94/0x348)

[ 1863.427093] [<8002c3f4>] (do_fork+0x94/0x348) from [<8000e080>] (ret_fast_sys                                                                                        call+0x0/0x30)

[ 1863.435453] Code: e7964004 e3540000 0a00001f e5953014 (e794c003)

[ 1863.441624] xhci_hcd 0000:01:00.0: ERROR Transfer event TRB DMA ptr not part                                                                                         of current TD

[ 1863.450042] ---[ end trace 2a826d12562d7983 ]---

[ 1863.841496] Unable to handle kernel NULL pointer dereference at virtual addre                                                                                        ss 000000dd

[ 1863.849631] pgd = d8e54000

[ 1863.852386] [000000dd] *pgd=68683831, *pte=00000000, *ppte=00000000

[ 1863.858741] Internal error: Oops: 17 [#6] PREEMPT SMP ARM

[ 1863.864154] Modules linked in: smsc95xx usbnet wlcore_sdio mxc_dcic

[ 1863.870548] CPU: 0 PID: 1100 Comm: DIO Tainted: G      D      3.10.53-ge55b1c                                                                                        e #13

[ 1863.878137] task: d87fe400 ti: d90e0000 task.ti: d90e0000

[ 1863.883572] PC is at kmem_cache_alloc+0x68/0x1a8

[ 1863.888213] LR is at kmem_cache_alloc+0x4c/0x1a8

[ 1863.892850] pc : [<800cf76c>]    lr : [<800cf750>]    psr: 200f0013

[ 1863.892850] sp : d90e1ec0  ip : 00000000  fp : d948f964

[ 1863.904345] r10: d948f800  r9 : 04ddf048  r8 : d90e0000

[ 1863.909585] r7 : 000000d0  r6 : 010e6000  r5 : d8001f00  r4 : 000000dd

[ 1863.916126] r3 : 00000000  r2 : 00000001  r1 : 000000d0  r0 : 00000000

[ 1863.922672] Flags: nzCv  IRQs on  FIQs on  Mode SVC_32  ISA ARM  Segment user

[ 1863.929822] Control: 10c53c7d  Table: 68e5404a  DAC: 00000015

[ 1863.935583] Process DIO (pid: 1100, stack limit = 0xd90e0238)

[ 1863.941344] Stack: (0xd90e1ec0 to 0xd90e2000)

[ 1863.945724] 1ec0: 003d0f00 d90e0028 80d93780 80d48ba8 d8bf03c4 73dff4b8 d948f                                                                                        800 80047588

[ 1863.953924] 1ee0: 80d91f10 73dfef88 00000000 8004fd2c 00000000 80d48b50 d8fd4                                                                                        000 d8fd5fb0

[ 1863.962122] 1f00: d948f800 003d0f00 d90e0028 80d93780 80d48ba8 d8bf03c4 73dff                                                                                        4b8 d948f800

[ 1863.970320] 1f20: d948f964 8002bd04 d948f9dc 00000000 73dfef88 00000000 00010                                                                                        000 80d380c0

[ 1863.978519] 1f40: 000262e0 00000000 80d476e8 003d0f00 00020200 00000000 00000                                                                                        000 73dff4b8

[ 1863.986717] 1f60: d90e0000 00000000 01976198 8002c3f4 00000000 00000000 00000                                                                                        000 f4a00100

[ 1863.994916] 1f80: 73dfef90 8000e94c 73dff4b8 76f4f178 00000000 00000078 8000e                                                                                        204 d90e0000

[ 1864.003114] 1fa0: 00000000 8000e080 73dff4b8 76f4f178 003d0f00 73dfef88 73dff                                                                                        4b8 73dff910

[ 1864.011313] 1fc0: 73dff4b8 76f4f178 00000000 00000078 73dfef90 73dff450 73dff                                                                                        684 01976198

[ 1864.019511] 1fe0: 003d0f00 76fd2348 76f3451d 7618afe6 200f0030 003d0f00 00000                                                                                        000 00000000

[ 1864.027741] [<800cf76c>] (kmem_cache_alloc+0x68/0x1a8) from [<80047588>] (all                                                                                        oc_pid+0x18/0x4ac)

[ 1864.036477] [<80047588>] (alloc_pid+0x18/0x4ac) from [<8002bd04>] (copy_proce                                                                                        ss.part.55+0x85c/0xe8c)

[ 1864.045637] [<8002bd04>] (copy_process.part.55+0x85c/0xe8c) from [<8002c3f4>]                                                                                         (do_fork+0x94/0x348)

[ 1864.054631] [<8002c3f4>] (do_fork+0x94/0x348) from [<8000e080>] (ret_fast_sys                                                                                        call+0x0/0x30)

[ 1864.063007] Code: e7964004 e3540000 0a00001f e5953014 (e794c003)

[ 1864.069352] ---[ end trace 2a826d12562d7984 ]---

[ 1865.844231] Unable to handle kernel NULL pointer dereference at virtual addre                                                                                        ss 000000dd

[ 1865.852438] pgd = d8f24000

[ 1865.855166] [000000dd] *pgd=68df9831, *pte=00000000, *ppte=00000000

[ 1865.861574] Internal error: Oops: 17 [#7] PREEMPT SMP ARM

[ 1865.866985] Modules linked in: smsc95xx usbnet wlcore_sdio mxc_dcic

[ 1865.873335] CPU: 0 PID: 565 Comm: haproxy Tainted: G      D      3.10.53-ge55                                                                                        b1ce #13

[ 1865.881168] task: d8e00000 ti: d89fa000 task.ti: d89fa000

[ 1865.886582] PC is at kmem_cache_alloc+0x68/0x1a8

[ 1865.891203] LR is at kmem_cache_alloc+0x4c/0x1a8

[ 1865.895824] pc : [<800cf76c>]    lr : [<800cf750>]    psr: 20070013

[ 1865.895824] sp : d89fbef8  ip : d6a96480  fp : 00000007

[ 1865.907302] r10: 80d872c0  r9 : 04ddf048  r8 : d89fa000

[ 1865.912528] r7 : 000000d0  r6 : 010e6000  r5 : d8001f00  r4 : 000000dd

[ 1865.919058] r3 : 00000000  r2 : 00000001  r1 : 000000d0  r0 : 00000000

[ 1865.925590] Flags: nzCv  IRQs on  FIQs on  Mode SVC_32  ISA ARM  Segment user

0 Kudos
1 Reply

474 Views
igorpadykov
NXP Employee
NXP Employee

Hi Awadhesh

reason may be ddr errors, one can retest board using ddr test

https://community.freescale.com/docs/DOC-105652

or broken smsc95x chip, to check this one can remove its driver

from image and test.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos