Hi,
I'm using MCF54418 processor with MQX 4.0 and CodeWarrior 10.6. I need to add WL1835 wifi module from Texas Instruments and connect it with SPI. There is no driver for this module but there are few drivers to other wifi modules (Atheros, RedPine, GainSpan). I think I can use one of this and add few changes to it to driver can works with my module. Is there might be any problem with this? Which driver would be most suitable for this. I'm new in MQX and drivers. Do you have any suggestions?
Thanks
Hello,
Unfortunately I can provide a comprehensive answer. You need to create your own driver for the WL1835.
If you want to use the (Atheros, RedPine, GainSpan) modules as reference, you need to compare the features, specifications, functional description and electrical characteristics in order to choose the best option. Unfortunately I can help with that.
For more information about the Atheros, RedPine, GainSpan modules please check the below links:
http://cache.freescale.com/files/wireless_comm/doc/data_sheet/AR4100P_DATASHEET.pdf
http://www.redpinesignals.com/Chipsets/IoT/RS9110.php
http://cache.freescale.com/files/soft_dev_tools/doc/support_info/GS_WiFiDriver.pdf
In order to create a new MQX driver please check the below links:
https://community.freescale.com/docs/DOC-102588
Have a great day,
Sol
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------