SCI on MC9S12XEQ512 not working without PE micro BDM cable and Hiwave

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SCI on MC9S12XEQ512 not working without PE micro BDM cable and Hiwave

420 Views
dakotabassett
Contributor I

I have encountered a problem while trying to test and SCI module on my micro. It works fine with the BDM cable attached and Hiwave running, it requires both to function. As soon as I disconnect the BDM cable or close hiwave the SCI immediately stops transmitting. I am transmitting from SCI0 to SCI1 every 20 milliseconds.

Labels (1)
0 Kudos
2 Replies

317 Views
dakotabassett
Contributor I

Is there any relationship between the two that I am not understanding?

0 Kudos

317 Views
iggi
NXP Employee
NXP Employee

Hi,

see answer to the following topic, it is very much the same as to this one:

https://community.freescale.com/thread/352246

Regards,

iggi

0 Kudos