lan8720 (RMII) with imx6Q(L3.0.35_4.1.0)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

lan8720 (RMII) with imx6Q(L3.0.35_4.1.0)

5,765 Views
pfsang
Contributor IV

Hi,

I connected a lan8720 (RMII) with imx6Q. We use the GPIO 16 as clock output for the phy.

i used the following the patch to my kernel. 

Re: iMX6 RGMII + ENET_REF_CLK/ENET_TX_CLK

But in both of uboot and kernel , the phy does not work and the link led also does not light.

because the RST pin of lan8720a on our board is connected with POR_B of imx6 control ,

it can't not be set to GPIO. i use soft reset to reset phy.

8720a.JPG.jpg

Here is my iomux config:

board_mx6q_XXX.h file

----------------------------------------------------------------------

/* ENET */

MX6Q_PAD_ENET_MDIO__ENET_MDIO,

MX6Q_PAD_ENET_MDC__ENET_MDC,

MX6Q_PAD_ENET_RXD0__ENET_RDATA_0,

MX6Q_PAD_ENET_RXD1__ENET_RDATA_1,

MX6Q_PAD_ENET_CRS_DV__ENET_RX_EN,

MX6Q_PAD_ENET_TXD0__ENET_TDATA_0,

MX6Q_PAD_ENET_TXD1__ENET_TDATA_1,

MX6Q_PAD_ENET_TX_EN__ENET_TX_EN,

MX6Q_PAD_GPIO_16__ENET_ANATOP_ETHERNET_REF_OUT,

MX6Q_PAD_ENET_RX_ER__ENET_RX_ER,

-------------------------------------------------------------------------

My fec init procedure:

board_mx6q_XXX.c file

----------------------------------------------------------------------

static int mx6q_8720_fec_phy_init(struct phy_device *phydev)

{

     int val;

     mxc_iomux_set_gpr_register(1, 21, 1, 1);

     /* reset phy */

     val = phy_read(phydev, 0x0);

     phy_write(phydev, 0x0, (val |BMCR_RESET));

    

     msleep(10);

     val = phy_read(phydev, 0x0);

     if (val & BMCR_PDOWN) {

phy_write(phydev, 0x0, (val & ~BMCR_PDOWN));

     }

     return 0;

}

--------------------------------------------------------


Please give me a suggestion or idea.

B&R

peter.cao

Labels (5)
0 Kudos
12 Replies

1,542 Views
pfsang
Contributor IV

hi all,

    i have solved the problem.

    the crash problem is If no phy detect, i open the eth interface, it is not reasonable.

    the cause that no phy detected when power-on is the sending phy clk is after phy detect.

    so i manually enable enet_clk at mx6_clocks_init() , and the problem is solved.

0 Kudos

1,544 Views
samuel-park
Contributor I


Could you share the code that how to fixed this issue?

thanks.


0 Kudos

1,544 Views
desmond_2014
Contributor I

could you share the code that how to fixed this issue?thanks

0 Kudos

1,544 Views
pfsang
Contributor IV

during debug, i found the following log error:

eth0: no PHY, assuming direct connection to switch

PHY 0:00 not found

eth0: could not attach to PHY

IP-Config: Failed to open eth0

IP-Config: No network devices available.

i traced the code and found  it does not find the attached phy in fep->mii_bus->phy_map in fec_enet_mii_probe function (fec.c),

the map is null. 

do anyone know why the map is null?

0 Kudos

1,544 Views
igorpadykov
NXP Employee
NXP Employee

Hi fang

I think that connection nRST to POR is not good.

Because LAN8720 VDD1A,VDD2A,VDDIO are turned ON

later in software, such configuration is used on Freescale designs.

Probably for that reason you see "PHY not found" error.

Actually you can check with SDK LAN8720 example, if processor can

detect PHY.

"MX6_PLATFORM_SDK "

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6Q&nodeId=018rH3ZrDRB24A&fpsp=1&t...

Best regards

chip

0 Kudos

1,544 Views
pfsang
Contributor IV

hi, chipexpert

        my link led has lighted and it can find out phy and got ip.

        but now i encounter a new problem.

        when the power on,  it can not find out phy . and when i input the "ifconfig eth0 up", the kernel dumped.

        but when i input reboot cmd, it can find out phy and got ip after reboot.

        i trace the source and found it hangs on  napi_enable(&fep->napi);; in fec_enet_open function (fec.c)

        how to fix it?

----------------------------------------------------------------------------------------------

kernel BUG at include/linux/netdevice.h:520!

Unable to handle kernel NULL pointer dereference at virtual address 00000000

pgd = b29f4000

[00000000] *pgd=429c5831, *pte=00000000, *ppte=00000000

Internal error: Oops: 817 [#1] PREEMPT SMP

Modules linked in:

CPU: 1    Not tainted  (3.0.35 #28)

PC is at __bug+0x1c/0x28

LR is at __bug+0x18/0x28

pc : [<8004068c>]    lr : [<80040688>]    psr: 40000013

sp : b28b1df0  ip : 80035f40  fp : 00000000

r10: b22a8fc0  r9 : 00000000  r8 : b21abf0c

r7 : b201b044  r6 : 00000000  r5 : b201b000  r4 : b201b000

r3 : 00000000  r2 : 00000001  r1 : 80a75d18  r0 : 00000033

Segmentation faultFlags: nZcv  IRQs on  FIQs on  Mode SVC_32  ISA ARM  Segment user

Control: 10c53c7d  Table: 429f404a  DAC: 00000015

..........

[<8004068c>] (__bug+0x1c/0x28) from [<802f83d8>] (fec_enet_open+0x3b8/0x480)

[<802f83d8>] (fec_enet_open+0x3b8/0x480) from [<80422868>] (__dev_open+0xa0/0xf0)

[<80422868>] (__dev_open+0xa0/0xf0) from [<80422a90>] (__dev_change_flags+0x7c/0x134)

[<80422a90>] (__dev_change_flags+0x7c/0x134) from [<80422bb4>] (dev_change_flags+0x10/0x48)

[<80422bb4>] (dev_change_flags+0x10/0x48) from [<80474a1c>] (devinet_ioctl+0x77c/0x818)

[<80474a1c>] (devinet_ioctl+0x77c/0x818) from [<8040e844>] (sock_ioctl+0x68/0x260)

[<8040e844>] (sock_ioctl+0x68/0x260) from [<800fc0a0>] (do_vfs_ioctl+0x80/0x54c)

[<800fc0a0>] (do_vfs_ioctl+0x80/0x54c) from [<800fc5a4>] (sys_ioctl+0x38/0x5c)

[<800fc5a4>] (sys_ioctl+0x38/0x5c) from [<8003d000>] (ret_fast_syscall+0x0/0x30)

Code: e59f0010 e1a01003 eb1321bd e3a03000 (e5833000)

0 Kudos

1,544 Views
Sasamy
Contributor IV

Hi

int __init mx6_clocks_init(unsigned long ckil, unsigned long osc,

        unsigned long ckih1, unsigned long ckih2)

{

....

- -     pll8_enet_main_clk.disable(&pll8_enet_main_clk);

++     pll8_enet_main_clk.enable(&pll8_enet_main_clk);

Alexander

0 Kudos

1,544 Views
pfsang
Contributor IV

hi,

    i made a mistake about the bug.  the bug is not at clk_enable , is at i   napi_enable(&fep->napi)( fec_enet_open ).  do you know why it will crash?

0 Kudos

1,544 Views
Sasamy
Contributor IV

I think GPR1 register must be set before  imx6_init_fec()

static void __init xxx_board_init(void)

{

...

++    mxc_iomux_set_gpr_register(1, 21, 1, 1);

    imx6_init_fec(fec_data);

not in function

static int mx6q_8720_fec_phy_init(struct phy_device *phydev)

{

    int val;

--    mxc_iomux_set_gpr_register(1, 21, 1, 1);

as in your example

Alexander

0 Kudos

1,544 Views
pfsang
Contributor IV

hi Alexander

    thank you for your reply.  i will try it tomorrow

0 Kudos

1,545 Views
igorpadykov
NXP Employee
NXP Employee

Hi fang

nRST is hardware reset and this signal latches hardware LAN8720 configuration

(MODE[] signals), seems it is not possible to set it with software reset.

I would suggest to apply to LAN8720 vendor (SMSC) tech

support for workaround.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

1,545 Views
pfsang
Contributor IV

hi, chipexpert

         we connect nRst pin with POR_B , which is global reset. when power on, pmic willl reset imx6 and others peripherals included lan8720a.   seems i needn't to set it with soft reset .

          is that right ?

0 Kudos