Add a new characteristic to weather service in the weather station project

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Add a new characteristic to weather service in the weather station project

1,582 Views
sidi_namou1996
Contributor I

Hello,

I am using the BLE of rapid iot kit to send 6 data to my android application, however i could not find any document that can help me to create my own service, therefore, i used the weather station project which has a wheather service that send 2 data( temperature and humidity) via BLE, so i have tried to understand how it works but the problem is that the main MCU send serial commands to the MKW41Z MCU and there is no document that gives you an information about this serial communication. 

Besides here, i tried to add the pressure characteristic to send my third data but i found an issue that every special characteristic has a special value format and a special adress (identifier)(like temperature it has a particular format value  and 0x2A1C as identifier).

So my question is:

is there any document that can help me to create my own service and my own characteristic????

if not please give me a document that contains all of acceptable characteristic because i sought every where and i did not find anything helpful.

Labels (1)
0 Kudos
1 Reply

1,526 Views
Sebastian_Del_Rio
NXP Employee
NXP Employee

Hi, I hope you're doing well!

 

The Rapid IoT Kit is using two MCUs to operate. The main device is a K64 MCU, while the one managing wireless connectivity is a KW41Z. These two communicate using FSCI commands.

 

Still, having said this, the development of applications for the Rapid IOT kit has migrated to the Atmosphere IoT Studio. Could you please take a look at the available documentation page for Atmosphere IoT Studio, here?

 

Best regards,

Sebastian

0 Kudos