Debian packages on imx8m mini evk linux image

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Debian packages on imx8m mini evk linux image

4,564 Views
Chayma
Contributor III

Hello everyone,

I have been stuck for days. I couldn't install debian packages using apt-get.

Even I added the apt-get command in the linux image, I couldn't install any of the packages.

I want to install scipy using pip and failed because there are some libraries package that should be installed like

libatlas-base-dev and gfortran

Could anyone help ?

And if there is a complete debian image for the evk ?

Thank you in advance.

Best regards,

2 Replies

4,452 Views
igorpadykov
NXP Employee
NXP Employee

Hi Chayma

unfortunately nxp does not officially support debian, one can look at third party:

https://boundarydevices.com/wiki/debian-for-nitrogen8/ 

https://boundarydevices.com/ubuntu-bionic-18-04-lts-for-nitrogen8m-board-september-2018-kernel-4-9-x... 

or Build Ubuntu For i.MX8 Series Platform 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

4,452 Views
Chayma
Contributor III

Thank you for your answer. I will look for the links you provided me.

0 Kudos