Hi Dear Reader(s),
I am trying to exercise the memory protection unit functions, but anything that I changed the descriptor would take the codes to HardFault_Handler(). See line 116 to line 122 in the main.c from the attached file. These lines are copied below.
// Descriptor 0
// MPU->RGD[0].WORD0 = 0x1FFF8000; // start address
// MPU->RGD[0].WORD1 = 0x20000000; // end address
// MPU->RGD[0].WORD2 = 0x61f7df; // access R/W for masters: M7 - M0
// // 0x7df;
// //0x61f7df reset value suggests there are M3 - M0 masters.
// MPU->RGD[0].WORD3 = 1; // optional PID, PIDMask, Valid
I have also tried to write back what were in these registers, the mcu would go to HardFault_Handler().
Is there anything I need to change to enable the write to region descriptors?
Thanks,
Kevin
PS. attached zip file.
Hi Kevin,
Please have a look at this thread:
https://community.nxp.com/message/1158836
Thanks,
BR, Daniel
Hi Kevin,
If I understand, you want to restrict the core access (write and read) in Descriptor 5.
You write:
MPU->RGD[5].WORD2 = 0x7c0;
Which means:
[4-3] M0SM = 0b00 r/w/x; read, write and execute allowed.
It should be
MPU->RGD[5].WORD2 = 0x7D8;
[4-3] M0SM = 0b11 Same as User mode defined in M0UM
[2-1] M0UM = 0b000 An attempted access of that mode may be terminated with an access error (if not allowed by
another descriptor) and the access not performed.
But looking at Descriptor 0 and the core access rights in the Supervisor mode, I see that you allows the core to access the whole map.
So, the descriptor 5 won't trigger anyway.
Regards,
Daniel
Hi Daniel,
Thank you very much for your helps, I can set up the MPU now.
When I looked at the EAR/EDR, and I could NOT find the exact address that caused the error.
1) Block write access
MPU->RGDAAC[0] = 0x7dd; // restrict the write access
*(unsigned int *)0x20004000 = 0xAABBCCDD; or
*(unsigned int *)0x20006000 = 0xAABBCCDD;
CESR[SPERR3] = 1
Hi Daniel,
I have changed all RGDs so that only Debugger is allowed to access the memory.
And I used these lines to test.
*(unsigned int *)0x20006000 = 0xAABBCCDD;
temp = *(unsigned int *)0x20006000;
I just do not understand why the codes can NOT go to HardFault_Handler().
Please find the attached and run it.
Is there anything that I have missed?
Thanks,
Kevin