How to Change the virtual channel in imx8

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to Change the virtual channel in imx8

1,656 Views
vimalan_93
Contributor I

Hi

I am using rocko(kernel version: 4.9.88) distribution in  yacto BSP for IMX8M EVK board with default ov5640 camera. Currently the default camera uses the virtual channel zero for receiving the mipi data.

I have two questions,

  1. How to change the virtual channel? Where do i need to modify in kernel source? 
  2. Can imx8 receive the data from VC0 & VC1 simultaneously? if yes, what is the procedure to do that.?

Thanks & Regrads,

Vimal

Labels (1)
Tags (1)
0 Kudos
2 Replies

1,224 Views
vimalan_93
Contributor I

Hi igorpadykov

Thanks for the response.

Regards

Vimal.

0 Kudos

1,224 Views
igorpadykov
NXP Employee
NXP Employee

Hi Vimal

For i.MX8M MIPI virtual channel is not used, so the driver will not split the video from each virtual channel.

For dual camera one can check

Dual camera support for i.MX8M EVK 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos