S12Z - Simulating ECC errors at RAM by debug access

Document created by Radek Sestak Employee on May 11, 2017Last modified by Radek Sestak Employee on Jan 16, 2020
Version 4Show Document
  • View in full screen mode

For debug purposes, it is possible to read and write the user data and

the ECC value directly from/to the SRAM memory. For these debug accesses a register

interface is available.

 

By the debug access and writing incorrect data + ECC values into the system memory, 

the single and double bit ECC errors may be simulated for checking the software error handling.

 

The debug registers may be modified only in a special mode.

 

The tested address 0x3000 is excluded from linker use - see prm linker file.

 

I hope it helps you.

Radek

3 people found this helpful

Attachments

Outcomes