Example MPC5646C eMIOS frequency measurement CW210

Document created by Petr Stancik Employee on May 3, 2017Last modified by ebiz_ws_prod on Dec 13, 2017
Version 3Show Document
  • View in full screen mode

********************************************************************************
* Detailed Description:
*
* This example shows possible implementation of frequency and duty cycle

* measurement with the help of eMIOS module.
* Two eMIOS channels are used and set to IPWM and IPM modes. The first channel
* measures the positive pulse width and the second channel measures the period.
*
* EVB connection:
* PJ7.5 to PJ7.6 ... connect external pulse signal to this
*
* See result on PC terminal (9600, 8N1)
* ------------------------------------------------------------------------------
* Test HW:  XPC56xxMB2 + XPC564xB/C, SPC5646C 0N32E silicon
* Target :  internal_FLASH, RAM
* Fsys:     120 MHz PLL0
* Debugger: Lauterbach Trace32. script for internal_FALSH run_from_flash.cmm
*                               script for RAM: run_from_ram_vle.cmm
*
********************************************************************************

 

 

BR, Petr

Original Attachment has been moved to: Example-MPC5646C-eMIOS-IPM-IPWM-v1.0-CW210.zip

9 people found this helpful

Attachments

    Outcomes