このウィジェットは表示できません。
このウィジェットは表示できません。
このウィジェットは表示できません。
このウィジェットは表示できません。
このウィジェットは表示できません。

SPI Transfer in Interrupt mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SPI Transfer in Interrupt mode

880件の閲覧回数
nhuan_huynhduc2
Contributor II

Hello everyone,

Now, I am working on the SPI module in S32K144 EVB, and I would like to transfer data based on interrupt. But I can not find any examples.

Could you provide me a basic example of SPI transfer in interrupt mode?

Thank you so much. <3

ラベル(1)
0 件の賞賛
3 返答(返信)

788件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Nhuan Huynh Duc,

Please download the latest S32 Design Studio for ARM 2.2 – Windows/Linux(REV 2.2), then you can refer the spi_pal_s32k144 example.

spi_pal_s32k144.png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛

788件の閲覧回数
nhuan_huynhduc2
Contributor II

Hi Robin,

I have already referred to this example, but it's not suitable for my case.

Do you have an example is similar to LPSPI_s32k144 ? 

pastedImage_1.png

Thank you

0 件の賞賛

788件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

There are only three lpspi examples in S32SDK S32K1xx RTM v3.0.0:

LPSPI.png

LPSPI Transfer.png

LPSPI DMA.png

It seem that there is no LPSPI_s32k144 example in S32 Design Studio for ARM 2.2.

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------