i.MXRT1064 Power Issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MXRT1064 Power Issue

405 Views
dipesh
Contributor I
Hi all, I am using i.MXRT1064. While we power up processor, voltage doesn't appears across DCDC_OUT net (LDO). I have gone through multiple similar threads in this forum and also through power up sequence given in hardware reference manual. During debug we have found that except DCDC_Out net all other voltages are working. CLK is working. PMIC_ON_REQ is 0.9V. Can anyone help regarding this? pl. give more detail regarding PMIC_ON_REQ signal. Thanks, Dipesh
0 Kudos
1 Reply

388 Views
FelipeGarcia
NXP Employee
NXP Employee

Hi Dipesh,

Could you please share how are your connections for DCDC_OUT? Additionally, please also make sure that:

1) DCDC turn-ON sequence is implemented in firmware as per reference manual topic 18.6.1.

2) PSWITCH and PMIC_ON_REQ are both high (Because it's mandatory to be high to enable DCDC). You can refer to our board schematics to see appropriate connections.

3) 1ms delay (reset time) is provided to enable DCDC after DCDC_IN powered up.

Best regards,

Felipe

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored. Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

------------------------------------------------------------------------------ 

0 Kudos