i.MX RT1170 can use Gigabit Ethernet to do MAC to MAC without PHY

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX RT1170 can use Gigabit Ethernet to do MAC to MAC without PHY

Jump to solution
1,294 Views
WJC
Contributor I

Hello,

I want to use the Gigabit Ethernet to do MAC to MAC without PHY (RGMII to RGMII) on RT1170.
Does this work?

 

0 Kudos
1 Solution
1,218 Views
danielchen
NXP TechSupport
NXP TechSupport

Yes, ENET 10/100Mbps can use MAC-to-MAC without phy.  But only RMII interface can support it.

 

Regards

Daniel

View solution in original post

0 Kudos
4 Replies
1,234 Views
WJC
Contributor I


ENET 10/100Mbps can use MAC-to-MAC without phy.

Attached the simple block diagram.

Thanks in advance.

WJC

0 Kudos
1,219 Views
danielchen
NXP TechSupport
NXP TechSupport

Yes, ENET 10/100Mbps can use MAC-to-MAC without phy.  But only RMII interface can support it.

 

Regards

Daniel

0 Kudos
1,211 Views
WJC
Contributor I

Thanks for your reply.

0 Kudos
1,263 Views
danielchen
NXP TechSupport
NXP TechSupport

@WJC 

 

RT1170 does not support MAC TO MAC connection without PHY.  Because RT1170 doesn't have delay line inserted on rx/tx data sampling capturing path, so timing will not match.

 

Regards

Daniel