i.MX RT1170 - MII interface signal RX_DV is missing in pin list

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX RT1170 - MII interface signal RX_DV is missing in pin list

764 Views
bernhardfink
NXP Employee
NXP Employee

I can't find the RX_DV signal on the i.MX RT1170, which is defined for the ethernet MII interface. (checked in the Data Sheet as well as in the Config Tool).

Is it supposed to be there or is it missing by purpose for one or the other reason?

Regards,
Bernhard.

0 Kudos
1 Reply

746 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
In the RM, it uses the MII_RXDV to explain the MII interface, however, in Table 60-45. ENET External Signals, it uses the RX_EN instead of the MII_RXDV, it definitely will confuse the developers, so I'll report the error to the Document team for further checking.

jeremyzhou_0-1627886502060.png

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos