i.MX RT106F with 8080 panel

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX RT106F with 8080 panel

484 次查看
kentseng
Contributor II

Dear Sir

We develop a project using RT106F, but the LCM panel with 8080, 

have any RT106x with 8080 panel interface connection and example code?

标签 (1)
标记 (2)
0 项奖励
1 回复

478 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Have any RT106x with 8080 panel interface connection and example code?
-- Whether you want to RT106x to connect the LCD panel via the 8080 interface, if yes, please refer to the application note for details.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

0 项奖励