can M7 and M4 access flexspi A at the same time

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

can M7 and M4 access flexspi A at the same time

459 次查看
xjy198903
Contributor III

In rt1176 board, can M7 and M4 access flexspi A at the same time? Will there be any data anomalies? If not, how to deal with the data synchronization problem

0 项奖励
4 回复数

432 次查看
Masmiseim
Senior Contributor I

Depends,

you can execute Code from the external Flash (XiP) from both cores simultaneously. The Hardware takes care of the synchronization.

If you like to read/write manually on the interface, then you have to do a synchronization.

0 项奖励

428 次查看
xjy198903
Contributor III
I want to read/write manually on the interface, how can i do a synchronization? Could you give some advice or examples?
0 项奖励

390 次查看
Masmiseim
Senior Contributor I

I’m not aware of an out of the box solution.

You could check the MessageBox Unit of the Controller to communicate between the two cores. Or use a shared memory based communication.

368 次查看
xjy198903
Contributor III
Hi, Masmiseim
I will try to use sema4 to complete data synchronization, thank you very much
0 项奖励