are i.MX RT 1170 family ASIL(ISO 26262)/SIL(IEC 61508) compliancy level ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

are i.MX RT 1170 family ASIL(ISO 26262)/SIL(IEC 61508) compliancy level ?

828 Views
Kiyasul
Contributor I

1. ASIL and SIL compliancy level for industrial and automotive ? ASIL-B/C/D and SIL-2/3 ? Do you have plans in the future to get these compliancy certificates ? or do you already have them ? 

2. Also,

It says temperature gradient from

-40 to +125 for Automotive Part Number under i.MX RT 1171/72 which is AEC-Q100 Grade 1 requirements.

Please let me know if there are any plans for AEC-Q100 Grade 1 compliance for the i.MX RT 1171/72 family ? Or do you already have it ? This is required for an automotive OEM.

Tags (1)
0 Kudos
4 Replies

754 Views
NaiaraU
Contributor I

Hello jingpan,

And for auronautic market. Can we use it in a DALB/DALC applications?

 

0 Kudos

738 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi,

No, RT1170 hasn't such certification.

 

Regards,

 

0 Kudos

804 Views
Kiyasul
Contributor I

Thank you for the response

0 Kudos

809 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @Kiyasul ,

The i.MX RT 1170 auto PNs are qualified to AEC-Q100 Grade 3 with PPAP. However, the documents you need are shared under NDA with your nearest distributor.

i.MX RT1170 (Auto version) isn't a ASIL rated device but QM. As a QM device, it only can be used in ASIL A/B system/application, cannot support ASIL D application.

 

Regards,

Jing

0 Kudos