Why necessary to measure VOLT_DCB on MIMXRT1060-EVK/ FRDM-MC-LVPMSM?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Why necessary to measure VOLT_DCB on MIMXRT1060-EVK/ FRDM-MC-LVPMSM?

Jump to solution
560 Views
Carlio
Contributor II
Hi there, I was wondering if measuring VOLT_DCB is necessary when running the provided example for AN12214SW? Should it not be enough by measuring the three phases (Iabc)? Best regards C
0 Kudos
1 Solution
551 Views
FelipeGarcia
NXP Employee
NXP Employee

Hi Carlio,

VOLT_DCB is the DC bus voltage and it is measured by ADC for the MC analog sensing. This is for feedback sensing needed by the FOC algorithm. You can learn more about this in this document.

Best regards,

Felipe

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored. Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

------------------------------------------------------------------------------ 

View solution in original post

1 Reply
552 Views
FelipeGarcia
NXP Employee
NXP Employee

Hi Carlio,

VOLT_DCB is the DC bus voltage and it is measured by ADC for the MC analog sensing. This is for feedback sensing needed by the FOC algorithm. You can learn more about this in this document.

Best regards,

Felipe

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored. Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

------------------------------------------------------------------------------