Switch from VDD_HIGH_IN to VDD_SNVS_IN of RT family

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Switch from VDD_HIGH_IN to VDD_SNVS_IN of RT family

跳至解决方案
1,107 次查看
fredfu
NXP Employee
NXP Employee

Hi,

      In RT1052 RM, there is a bit to control switch from VDD_HIGH_IN to VDD_SNVS_IN, could you help to provide detailed description of the controlling circuit?

   Capture.PNG

Best Regards,

Fred Fu

0 项奖励
1 解答
1,097 次查看
wayne_wang
NXP Employee
NXP Employee

it can be disabled only when VDD_SNVS_IN and VDD_HIGH_IN both powered.

在原帖中查看解决方案

0 项奖励
3 回复数
1,104 次查看
wayne_wang
NXP Employee
NXP Employee

there is a internal diode between VDD_HIGH_IN and VDD_SNVS_IN, and this switch has function only in VDD_HIGH_IN and VDD_SNVS_IN powered, otherwise, it will always enable.

0 项奖励
1,099 次查看
fredfu
NXP Employee
NXP Employee

Hi  Wayne,

    Thanks. Can the switch be disabled? if customer don't need the channel from VDD_HIGH_IN to VDD_SNVS_IN.

Best Regards,

Fred Fu

0 项奖励
1,098 次查看
wayne_wang
NXP Employee
NXP Employee

it can be disabled only when VDD_SNVS_IN and VDD_HIGH_IN both powered.

0 项奖励