Running RT1170 EVK 1G and 100M ports on Zephyr at the same time

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Running RT1170 EVK 1G and 100M ports on Zephyr at the same time

467件の閲覧回数
xuqincs
Contributor I

Hi,

Is it possible to use both 100M and 1G interfaces on RT1170 EVK at the same time on Zephyr?

I'm aware the 1G interface can use a 100M enet driver and get 100M speed, which is fine, but not able to get dhcp after enabling the enet1g node on DT, int-gpio, reset-gpio, etc are configured. Also, getting DT error if I enable enet and enet1g nodes at the same time. Zephyr seems already supports multi-enet interfaces, is there anything missing in the board DTS? We are using RT1170 EVK.

 

Thanks.

タグ(1)
0 件の賞賛
1 返信

425件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport
0 件の賞賛