Dear all
I am looking for this to work with MfgTool included in SDK middleware - unlike RT1064, the flashloader.srec is not included there, I tried to build myself from the example, but it doesn't work.
Please help.
Regards!
Ping
Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
Please check the attachment.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Thanks, Jeremy
I copied it to the OS firmware folder, together with boot_image.bin(compiled with header), also downloaded blhost and copied. Unfortunately still not working, I am only test with iled_Blinky example and EVK_RT1024. I wonder what is wrong, do you get it working?
I hope there is full release of this like for EVK_RT1064, because that is working for me.
Urgently need to get it into production, please advise!
Regards!
Ping
Hi,
Thanks for your reply.
The MfgTool is a GUI tool, but it doesn't provide any log record that can indicate the failure reason.
So I'd like to suggest you to refer to the application note: AN12238 which illustrates how to use host-side command-line tools: SDPHost and Blhost to communicate with the Flashloader binary via USB-HID or UART.
The testing can help you to figure out the cause of failure and please give it a try.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------