MIMXRT1160-EVK with RK055HDMIPI4MA0 display

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MIMXRT1160-EVK with RK055HDMIPI4MA0 display

Jump to solution
1,120 Views
ACTC
Contributor I

Hi

I'm ordering the RT1160 eval kit and the suggested LCD display RK055HDMIPI4MA0. Best I can tell from the docs a 40 pin MIPI cable will be needed to connect the kit and the display. Is the cable included with the kit or display or do I need to get that separately.

Thanks

0 Kudos
Reply
1 Solution
1,113 Views
danielmilutinov
Contributor III

Hi,

According to MIMXRT1160-EVK Board User Manual, from here https://www.farnell.com/datasheets/3576931.pdf :

"If developers want to use LCD, NXP provides an optional LCD module RK055HDMIPI4M equipped with a 5.5” 720*1280 TFT LCD display with touch sensitive overlay. This module contains one FPC cable that connects to RT1160 EVK. The LCD interface can be connected to J48. LCD modules can be purchased from the NXP website."

That looks like a nice EVK and display, I think I'll order them as well to add to my collection!

View solution in original post

4 Replies
1,089 Views
ACTC
Contributor I

totally missed it but I see it now, that'll help for next time. thank you

0 Kudos
Reply
1,098 Views
ACTC
Contributor I

that's a big help thank you.

I cant find the data sheet you reference on the nxp dev kit landing page but if I search for it now that I have the doc id UM11617 I can find it.

thanks again

0 Kudos
Reply
1,093 Views
danielmilutinov
Contributor III

You're welcome, click on "SHOW ALL" in the documents section on the landing page https://www.nxp.com/design/development-boards/i-mx-evaluation-and-development-boards/i-mx-rt1160-eva... and it should be there. 

0 Kudos
Reply
1,114 Views
danielmilutinov
Contributor III

Hi,

According to MIMXRT1160-EVK Board User Manual, from here https://www.farnell.com/datasheets/3576931.pdf :

"If developers want to use LCD, NXP provides an optional LCD module RK055HDMIPI4M equipped with a 5.5” 720*1280 TFT LCD display with touch sensitive overlay. This module contains one FPC cable that connects to RT1160 EVK. The LCD interface can be connected to J48. LCD modules can be purchased from the NXP website."

That looks like a nice EVK and display, I think I'll order them as well to add to my collection!