Chip:MIMXRT1176
SDK Version:2.13.1
I've implemented SDK examples:lvgl_guider_cm7,and I don't want the screen to refresh everytime.
So I set disp_drv.full_refresh = 0 which means partial refresh mode in function lv_port_disp_init(),then the screen is mixed and flickering.
It seems to be related to the command and video mode,and the flush_cb should be modified?
How can I fix this?
Solved! Go to Solution.
Hi @Vinos ,
You can refer to this post.
https://blog.csdn.net/zhoutaopower/article/details/124600483
At the begin, it shows LVGL has three mode. It use first one. But RT1170 LVGL demo use the third and remove other two. I think it is because MIPI and LCD interface can't support partial display.
Regards,
Jing
I've seen a related post,NXP SDK doesn't support non-full-refresh mode?
https://forum.lvgl.io/t/imxrt1170-kits-updated-to-v8-running-only-full-refresh-mode/7829
Hi @Vinos ,
You can refer to this post.
https://blog.csdn.net/zhoutaopower/article/details/124600483
At the begin, it shows LVGL has three mode. It use first one. But RT1170 LVGL demo use the third and remove other two. I think it is because MIPI and LCD interface can't support partial display.
Regards,
Jing