I need to use the RT1176's PWM4 X,3 signal to control backlight intensity. Is there example code for setup of a PWM_X output? Something simple to get me started would be great. I'm using MCUXpresso and have enabled the PWM4 X,3 signal on GPIO_AD_21 configured as an output, but it doesn't look like the SDK 2.13.1 supports kPWM_PwmX as a signal channel for an output signal.
I did find this link where fsl_pwm.c was patched to provide PWM_X capability, but this hasn't worked for me either. I have also read this article but I'm still struggling.
Thank you.
Hi @mrd ,
What's the board you are using? The MIMXRT1170-EVK from NXP?
I think, we don't have the directly PWM_X example, but it is not difficult, you even can configure the register to realize it.
Anyway, tell me your used board and IDE, then I will find time to help you to check it on my side.
If you already write the related code, but can't work, just also upload it, I can help you to check it.
Best Regards,
kerry