IP Write to HyperRam on IMXRT1064

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IP Write to HyperRam on IMXRT1064

1,712 Views
etc
Contributor I

When using the ipwrite command to send data to HyperRam we find a multiple microsecond delay between the DUMMY_RWDS_DDR command and the WRITE_DDR command.  The delay only happens between CA and the first burst of data.  Is there an explanation for that delay?  Or some way to shorten it?

0 Kudos
2 Replies

1,691 Views
jay_heng
NXP Employee
NXP Employee

Do you see the same issue when using AHB write?

0 Kudos

1,637 Views
etc
Contributor I

I do not.  There is no delay between the DUMMY_RWDS command and the WRITE_DDR command in an AHB write. 

 

I do see a 15us delay between ahb write bursts that I assume is either the AHB_TX_BUF or the TX_FIFO  reloading.  It is difficult to ascertain what is going on between those two data sources.

0 Kudos