IMXRT1176 32MB QSPI flash problem during writing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMXRT1176 32MB QSPI flash problem during writing

1,667 Views
nxbg
Contributor I

Hi Team, we meet a strange problem, that we use Winbond W25Q256 Flash which is 32MB, but when we write 0x1000000, but the contents has been written to 0x30000000, it seems that it only accept 16MB, here is our FLASH configuration file:

#define FLASH_SIZE_KB 0x8000

flexspi_device_config_t deviceconfig = {
.flexspiRootClk = 100000000,
.flashSize = FLASH_SIZE_KB,
.CSIntervalUnit = kFLEXSPI_CsIntervalUnit1SckCycle,
.CSInterval = 2,
.CSHoldTime = 3,
.CSSetupTime = 3,
.dataValidTime = 0,
.columnspace = 0,
.enableWordAddress = 0,
.AWRSeqIndex = 0,
.AWRSeqNumber = 0,
.ARDSeqIndex = NOR_CMD_LUT_SEQ_IDX_READ_FAST_QUAD,
.ARDSeqNumber = 1,
.AHBWriteWaitUnit = kFLEXSPI_AhbWriteWaitUnit2AhbCycle,
.AHBWriteWaitInterval = 0,
};

 

Maybe I mistake for some configuration? Btw: I used SDRAM for debugging, so there is no XIP feature enable.

Thanks & Best Regards,

0 Kudos
4 Replies

1,658 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Maybe I mistake for some configuration?
-- To be prudent, I was wondering if you can list the LUT command table.
Further, please share the complete product number of the QSPI flash.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos

1,656 Views
nxbg
Contributor I
#define NOR_CMD_LUT_SEQ_IDX_READ_NORMAL 2 #define NOR_CMD_LUT_SEQ_IDX_READ_FAST 1 #define NOR_CMD_LUT_SEQ_IDX_READ_FAST_QUAD 0 // set it to index0 to align with xip settings #define NOR_CMD_LUT_SEQ_IDX_READSTATUS 3 #define NOR_CMD_LUT_SEQ_IDX_WRITEENABLE 4 #define NOR_CMD_LUT_SEQ_IDX_ERASESECTOR 5 #define NOR_CMD_LUT_SEQ_IDX_PAGEPROGRAM_SINGLE 6 #define NOR_CMD_LUT_SEQ_IDX_PAGEPROGRAM_QUAD 7 #define NOR_CMD_LUT_SEQ_IDX_READID 8 #define NOR_CMD_LUT_SEQ_IDX_WRITESTATUSREG 9 #define NOR_CMD_LUT_SEQ_IDX_ENTERQPI 10 #define NOR_CMD_LUT_SEQ_IDX_EXITQPI 11 #define NOR_CMD_LUT_SEQ_IDX_READSTATUSREG 12 #define CUSTOM_LUT_LENGTH 60 static uint32_t customLUT[CUSTOM_LUT_LENGTH] = { /* Normal read mode -SDR */ [4 * NOR_CMD_LUT_SEQ_IDX_READ_NORMAL] = FLEXSPI_LUT_SEQ(kFLEXSPI_Command_SDR, kFLEXSPI_1PAD, 0x03, kFLEXSPI_Command_RADDR_SDR, kFLEXSPI_1PAD, 0x18), [4 * NOR_CMD_LUT_SEQ_IDX_READ_NORMAL + 1] = FLEXSPI_LUT_SEQ(kFLEXSPI_Command_READ_SDR, kFLEXSPI_1PAD, 0x04, kFLEXSPI_Command_STOP, kFLEXSPI_1PAD, 0), /* Fast read mode - SDR */ [4 * NOR_CMD_LUT_SEQ_IDX_READ_FAST] = FLEXSPI_LUT_SEQ(kFLEXSPI_Command_SDR, kFLEXSPI_1PAD, 0x0B, kFLEXSPI_Command_RADDR_SDR, kFLEXSPI_1PAD, 0x18), [4 * NOR_CMD_LUT_SEQ_IDX_READ_FAST + 1] = FLEXSPI_LUT_SEQ( kFLEXSPI_Command_DUMMY_SDR, kFLEXSPI_1PAD, 0x08, kFLEXSPI_Command_READ_SDR, kFLEXSPI_1PAD, 0x04), /* Fast read quad mode - SDR */ [4 * NOR_CMD_LUT_SEQ_IDX_READ_FAST_QUAD] = FLEXSPI_LUT_SEQ(kFLEXSPI_Command_SDR, kFLEXSPI_1PAD, 0xEB, kFLEXSPI_Command_RADDR_SDR, kFLEXSPI_4PAD, 0x18), [4 * NOR_CMD_LUT_SEQ_IDX_READ_FAST_QUAD + 1] = FLEXSPI_LUT_SEQ( kFLEXSPI_Command_DUMMY_SDR, kFLEXSPI_4PAD, 0x06, kFLEXSPI_Command_READ_SDR, kFLEXSPI_4PAD, 0x04), /* Read extend parameters */ [4 * NOR_CMD_LUT_SEQ_IDX_READSTATUS] = FLEXSPI_LUT_SEQ(kFLEXSPI_Command_SDR, kFLEXSPI_1PAD, 0x81, kFLEXSPI_Command_READ_SDR, kFLEXSPI_1PAD, 0x04), /* Write Enable */ [4 * NOR_CMD_LUT_SEQ_IDX_WRITEENABLE] = FLEXSPI_LUT_SEQ(kFLEXSPI_Command_SDR, kFLEXSPI_1PAD, 0x06, kFLEXSPI_Command_STOP, kFLEXSPI_1PAD, 0), /* Erase Sector */ [4 * NOR_CMD_LUT_SEQ_IDX_ERASESECTOR] = FLEXSPI_LUT_SEQ(kFLEXSPI_Command_SDR, kFLEXSPI_1PAD, 0x20, kFLEXSPI_Command_RADDR_SDR, kFLEXSPI_1PAD, 0x18), /* Page Program - single mode */ [4 * NOR_CMD_LUT_SEQ_IDX_PAGEPROGRAM_SINGLE] = FLEXSPI_LUT_SEQ(kFLEXSPI_Command_SDR, kFLEXSPI_1PAD, 0x02, kFLEXSPI_Command_RADDR_SDR, kFLEXSPI_1PAD, 0x18), [4 * NOR_CMD_LUT_SEQ_IDX_PAGEPROGRAM_SINGLE + 1] = FLEXSPI_LUT_SEQ(kFLEXSPI_Command_WRITE_SDR, kFLEXSPI_1PAD, 0x04, kFLEXSPI_Command_STOP, kFLEXSPI_1PAD, 0), /* Page Program - quad mode */ [4 * NOR_CMD_LUT_SEQ_IDX_PAGEPROGRAM_QUAD] = FLEXSPI_LUT_SEQ(kFLEXSPI_Command_SDR, kFLEXSPI_1PAD, 0x32, kFLEXSPI_Command_RADDR_SDR, kFLEXSPI_1PAD, 0x18), [4 * NOR_CMD_LUT_SEQ_IDX_PAGEPROGRAM_QUAD + 1] = FLEXSPI_LUT_SEQ(kFLEXSPI_Command_WRITE_SDR, kFLEXSPI_4PAD, 0x04, kFLEXSPI_Command_STOP, kFLEXSPI_1PAD, 0), /* Read ID */ [4 * NOR_CMD_LUT_SEQ_IDX_READID] = FLEXSPI_LUT_SEQ(kFLEXSPI_Command_SDR, kFLEXSPI_1PAD, 0xAB, kFLEXSPI_Command_DUMMY_SDR, kFLEXSPI_1PAD, 0x18), [4 * NOR_CMD_LUT_SEQ_IDX_READID + 1] = FLEXSPI_LUT_SEQ(kFLEXSPI_Command_READ_SDR, kFLEXSPI_1PAD, 0x04, kFLEXSPI_Command_STOP, kFLEXSPI_1PAD, 0), /* Enable Quad mode */ [4 * NOR_CMD_LUT_SEQ_IDX_WRITESTATUSREG] = FLEXSPI_LUT_SEQ(kFLEXSPI_Command_SDR, kFLEXSPI_1PAD, 0x01, kFLEXSPI_Command_WRITE_SDR, kFLEXSPI_1PAD, 0x04), /* Enter QPI mode */ [4 * NOR_CMD_LUT_SEQ_IDX_ENTERQPI] = FLEXSPI_LUT_SEQ(kFLEXSPI_Command_SDR, kFLEXSPI_1PAD, 0x35, kFLEXSPI_Command_STOP, kFLEXSPI_1PAD, 0), /* Exit QPI mode */ [4 * NOR_CMD_LUT_SEQ_IDX_EXITQPI] = FLEXSPI_LUT_SEQ(kFLEXSPI_Command_SDR, kFLEXSPI_4PAD, 0xF5, kFLEXSPI_Command_STOP, kFLEXSPI_1PAD, 0), /* Read status register */ [4 * NOR_CMD_LUT_SEQ_IDX_READSTATUSREG] = FLEXSPI_LUT_SEQ(kFLEXSPI_Command_SDR, kFLEXSPI_1PAD, 0x05, kFLEXSPI_Command_READ_SDR, kFLEXSPI_1PAD, 0x04), };
0 Kudos

1,655 Views
nxbg
Contributor I

Here is attached LUT.txt and FLASH is W25Q256JVEIQ, my initialization code is here:

#ifndef XIP_EXTERNAL_FLASH
flexspi_device_config_t deviceconfig = {
.flexspiRootClk = 100000000,
.flashSize = CONFIG_FLASH_SIZE,
.CSIntervalUnit = kFLEXSPI_CsIntervalUnit1SckCycle,
.CSInterval = 2,
.CSHoldTime = 3,
.CSSetupTime = 3,
.dataValidTime = 0,
.columnspace = 0,
.enableWordAddress = 0,
.AWRSeqIndex = 0,
.AWRSeqNumber = 0,
.ARDSeqIndex = NOR_CMD_LUT_SEQ_IDX_READ_FAST_QUAD,
.ARDSeqNumber = 1,
.AHBWriteWaitUnit = kFLEXSPI_AhbWriteWaitUnit2AhbCycle,
.AHBWriteWaitInterval = 0,
};
#endif

static status_t flash_init_internal(void)
{
status_t status = kStatus_Success;

/* NOTE: Multithread access is not supported for SRAM target.
* XIP target MUST be protected by disabling global interrupts
* since all ISR (and API that is used inside) is placed at XIP.
* It is necessary to place at least "mflash_drv.o", "fsl_flexspi.o" to SRAM */
/* disable interrupts when running from XIP */
#ifdef XIP_EXTERNAL_FLASH
nxtos_uint32_t primask = __get_PRIMASK();

__asm("cpsid i");
#endif

#ifndef XIP_EXTERNAL_FLASH
flexspi_config_t config;

/* Get FLEXSPI default settings and configure the flexspi. */
FLEXSPI_GetDefaultConfig(&config);

/* Set AHB buffer size for reading data through AHB bus. */
config.ahbConfig.enableAHBPrefetch = true;
config.ahbConfig.enableAHBBufferable = true;
config.ahbConfig.enableAHBCachable = true;
config.rxSampleClock = kFLEXSPI_ReadSampleClkLoopbackFromDqsPad;
FLEXSPI_Init(MFLASH_FLEXSPI, &config);

/* AHB Read Address option bit. This option bit is intend to remove AHB burst start address alignment limitation */
MFLASH_FLEXSPI->AHBCR |= FLEXSPI_AHBCR_READADDROPT_MASK;

/* Configure flash settings according to serial flash feature. */
FLEXSPI_SetFlashConfig(MFLASH_FLEXSPI, &deviceconfig, kFLEXSPI_PortA1);
#endif

/* Update LUT table. */
FLEXSPI_UpdateLUT(MFLASH_FLEXSPI, 0, customLUT, CUSTOM_LUT_LENGTH);

#ifndef XIP_EXTERNAL_FLASH
/* Enter quad mode. */
status = flexspi_nor_enable_quad_mode(MFLASH_FLEXSPI);
#endif

/* Do software reset. */
FLEXSPI_SoftwareReset(MFLASH_FLEXSPI);

#ifdef XIP_EXTERNAL_FLASH
if (primask == 0)
{
__asm("cpsie i");
}
#endif

return status;
}

0 Kudos

1,645 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thanks for your reply and sharing.
After going through LUT.txt, I find that all LUT commands use the 3-byte address mode, however, for the W25Q256JV, it needs to use the 4-byte address mode to access the upper 16 MB partition.
I think it's the root cause.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------