IMXRT1050 - ENC - Test Register (55.9.1.16) - how to check the test signals?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMXRT1050 - ENC - Test Register (55.9.1.16) - how to check the test signals?

507 Views
Cindy
Contributor III

Hello,

I have used XBAR to connect the encoder signals from external pins to the on-board encoder module (phase A and phase B). I have also connected the external encoder signal-A to a quad timer to generate interupt and for signal processing.

XBARA_SetSignalsConnection(XBARA1, kXBARA1_InputIomuxXbarInout17, kXBARA1_OutputEnc1PhaseAInput);

XBARA_SetSignalsConnection(XBARA1, kXBARA1_InputIomuxXbarInout16, kXBARA1_OutputEnc1PhaseBInput);

XBARA_SetSignalsConnection(XBARA1, kXBARA1_InputIomuxXbarInout17, kXBARA1_OutputQtimer1Tmr0Input);

 

I am looking into this TEST REGISTER to generate the encoder signals for testing.

According to the manual:-

55.9.1.16.2 Function
The Test Register controls and sets the frequency of a quadrature signal generator; it
provides a quadrature test signal to the inputs of the quadrature decoder module.

Because I have used XBAR to connect ENC-Phase A to a quad timer, so, I am expecting interrupt would be generated when test mode (TEN) is enabled and period is set. But, I am not seeing this is happening.

Is there a way for me to check if the test signals are being generated?

 

Thanks!

 Best Regards,

Cindy

Labels (1)
0 Kudos
1 Reply

485 Views
CarlosGarabito
NXP TechSupport
NXP TechSupport

Hi @Cindy, which board are you using?

0 Kudos