Hi Team!
I'm using MIMXRT1170-EVK and I want to setup ADC_ETC/PWM sync mode with Config Tools.
I was using MIMXRT1060-EVK, but with i.MX1170, the appearance of Config Tools has changed, and there unknow terms, and I don't know how to set it like before.
Q.1 Following is the i.MX1060 ADC and ADC_ETC settings. How can I set it i.MX1170?
Q.2 Following is the setting screen of ADC_ETC of i.MX1170.
What was called a channel group and conversion control group in i.MX1060 has been replaced by Command ID and Trigger.
I read the reference manual, but I don't know how to set in actual.
I would like to see the setting screen when the ATC_ETC setting of Q1 is applied to i.MX1170.
Solved! Go to Solution.
Hi @kerryzhou -san
I was able to solve by myself.
By enabling the setting of the red frame in the figure below, ADC_ETC worked.
Hi @kenji ,
Please help to confirm two points:
1. When you use the CFG to configure the RT1060 ADC-ETC+ADC, it works on your side, right?
2. What's the CFG version you are using? Or from the MCUXPresso IDE? Which MCUXPresso IDE version.
Please give me more information at first, then I can help you to check more details.
Best Regards,
Kerry
Hi @kerryzhou -san
I will answer the question.
The following is the current situation.
I want to do same thing on i.MX1170.
Could you tell me how to set on Config Tools?
I would like to see the screen after end the settings on the i.MX1170.
Hi @kenji ,
Please also share me your working RT1060 configure file or the project, then I will help you to check more details in the RT1170.
Please keep patient, I need more time to do deeper checking, thanks.
Best Regards,
Kerry
Hi @kerryzhou -san
I was able to solve by myself.
By enabling the setting of the red frame in the figure below, ADC_ETC worked.
Hi @kerryzhou -san
I uploaded RT1062(MIMXRT1060-EVK) and RT1176(MIMXRT1170-EVK) board folder and .mex file.
Please check it.
By the way, is there any way to know why ADC_ETC_ERR interrupt happens?
I couldn't find out register that have ADC_ETC_ERR interrupt error flags.
I think, if I can know the reason for the error, it will help me to solve the problem.
Hi @kerryzhou -san
The following is the manual and setting screen of i.MX1170 regarding ADC_ETC.