Facing issue with LPC Link 2 with iMX RT 1170 Evk

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Facing issue with LPC Link 2 with iMX RT 1170 Evk

891 Views
Ankush_9881
Contributor II

I am trying to flash the code to iMX RT 1170 Evk using NXP MCU Boot utility. But I cannot find the USB HID device. Event though i followed the steps on

https://github.com/JayHeng/NXP-MCUBootUtility

Also I have checked with boot switches setting. 

Please can anyone help me ?

Thanks in advance!

0 Kudos
2 Replies

871 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello
Hope you are well.

How are you powering the EVK? If you are using the barrel connector(J43) make sure that that jumpers in J38 is in default position(1-2). If you want to power from the Freelink interface(J11) the jumper must be in position 5-6.

The USB interface for serial download is USB1, make sure you are using the correct interface:

Omar_Anguiano_0-1643671892537.png

 

Also, the SW1[3-4] need to be in position 01 for serial downloader.

If you have more questions do not hesitate to ask me.
Best regards,
Omar

855 Views
Ankush_9881
Contributor II

Thank you very much for the solution!

0 Kudos