Encrypted firmware via JTAG?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Encrypted firmware via JTAG?

719 Views
luishs
Senior Contributor I


Hi.

I have already solved the problems with JTAG and SWD.


One more question, please:

To upload an encrypted firmware image to RT1020, can I use Jlink through JTAG, or do I have to do it via USB with MFG Tools?

1 Reply

612 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

   To use encrypted boot the image should be loaded and run by boot ROM, using 

any available boot option. In this sense only the MFG may be used to work with HAB,

assuming other possible channels, such as JTAG are disabled or applied in secure

mode.  

 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!