Do you have an example of an RT1064 based web server?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Do you have an example of an RT1064 based web server?

797件の閲覧回数
join_ren
Contributor III

Dear NXP:

We need to development web server on RT1064. Do you have a example for reference?

Thanks for your support.

0 件の賞賛
2 返答(返信)

772件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
To provide the fastest possible support, I'd highly recommend you refer to the demo in the Lwip_examples in the SDK library for details.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛

792件の閲覧回数
mjbcswitzerland
Specialist V

Hi

See https://www.utasker.com/iMX/RT1064.html

i.MX RT 1064 dynamic web server with file system in internal QSPI, SD card or memory stick, with loading via FTP (and OTA firmware loading via HTTP).

Regards

Mark
[uTasker project developer for Kinetis and i.MX RT]
Contact me by personal message or on the uTasker web site to discuss professional training, solutions to problems or rapid product development requirements

For professionals searching for faster, problem-free Kinetis and i.MX RT 10xx developments the uTasker project holds the key: https://www.utasker.com/iMX/RT1064.html

0 件の賞賛