Hi All
We are doing some reliability testing and have identified a potential issue when testing on the MIMXRT1020EVK with regard to the DCDC converter.
The test consists of starting code that configures the DCDC to allow operation at 500MHz (setting 1.25V), running further code testing USB device operation and commanding a SW core reset so that the test repeats every (approx) 2s.
Typically after a few hundred such cycles the DCDC converter stabilising check spins for a long time, causing WDOG3 (used to monitor such issues) to fire and a further reset to be executed, after which it continues again normally. When the test is run for 2500 cycles the issue is seen maybe 10..15 times (to give an idea of its frequency).
The code is
DCDC_REG3 = ((DCDC_REG3 & ~DCDC_REG3_TRG_MASK) | DCDC_REG3_TRG_1_250V); // increase the DCDC voltage from default 1.15V to 1.25V
while ((DCDC_REG0 & DCDC_REG0_STS_DC_OK) == 0) { } // wait until the DCDC output stabilises
If WDOG3 timeout is set to a high value (like 30s) the hang is noticed and the attached debugger can be paused (it is in the while loop). The core registers show that the DCDC_REG0_STS_DC_OK was '0' when it was last checked but when the DCDC_REG0 register is viewed it is displayed as set.
Although the debugger can read registers, single stepping no longer works so it may be that the issue also has an effect on some other operation so it can't be known for sure that the DCDC stabilised and the code could continue or not.
The definition of the flag shows that the stabilisation is HW dependent:
but there is no further information about what is expected.
Since this happens on the MIMXRT1020EVK it may also be circuit design dependent and not happen on all HW.
Comments are welcome since this is very reproducible and somewhat worrying (although the WDOG3 does seem to always allow recovery after a delay).
Regards
Mark
For i.MX and Kinetis stock availability see https://www.utasker.com/Shop/semi.html
Hi @mjbcswitzerland ,
How did you implement the test code? is it just something like GPIO initialization and WDOG3 initialization with the following code in the end?
DCDC_REG3 = ((DCDC_REG3 & ~DCDC_REG3_TRG_MASK) | DCDC_REG3_TRG_1_250V); // increase the DCDC voltage from default 1.15V to 1.25V
while ((DCDC_REG0 & DCDC_REG0_STS_DC_OK) == 0) { } // wait until the DCDC output stabilises
Please kindly clarify.
Have a great day,
Kan
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi
Yes, this is the case
1. Set GPIO
2. Configure Watchdog
3. Change the DC/DC voltage <------------ sometimes hangs
4. Increase frequency from default to 528MHz
5. Start application code
6. After 2s command SW reset so it restarts at 1. again
Regards
Mark
Hi @mjbcswitzerland ,
Thanks for the clarification! Is it possible to share the code? I will try to reproduce it here, not sure if it is a board specific issue.
Have a great day,
Kan
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi
I have managed a fairly good improvement with the following change:
Originally the DCDC converter voltage change was performed in a single step:
DCDC_REG3 = ((DCDC_REG3 & ~DCDC_REG3_TRG_MASK) | DCDC_REG3_TRG_1_250V); // increase the DCDC voltage from default 1.15V to 1.25V
_WAIT_REGISTER_FALSE(DCDC_REG0, DCDC_REG0_STS_DC_OK); // wait until the DCDC output stabilises
but if it is instead performed in several small steps:
DCDC_REG3 = ((DCDC_REG3 & ~DCDC_REG3_TRG_MASK) | DCDC_REG3_TRG_1_175V);
_WAIT_REGISTER_FALSE(DCDC_REG0, DCDC_REG0_STS_DC_OK); // wait until the DCDC output stabilises
DCDC_REG3 = ((DCDC_REG3 & ~DCDC_REG3_TRG_MASK) | DCDC_REG3_TRG_1_200V);
_WAIT_REGISTER_FALSE(DCDC_REG0, DCDC_REG0_STS_DC_OK); // wait until the DCDC output stabilises
DCDC_REG3 = ((DCDC_REG3 & ~DCDC_REG3_TRG_MASK) | DCDC_REG3_TRG_1_225V);
_WAIT_REGISTER_FALSE(DCDC_REG0, DCDC_REG0_STS_DC_OK); // wait until the DCDC output stabilises
DCDC_REG3 = ((DCDC_REG3 & ~DCDC_REG3_TRG_MASK) | DCDC_REG3_TRG_1_250V); // increase the DCDC voltage from default 1.15V to 1.25V
_WAIT_REGISTER_FALSE(DCDC_REG0, DCDC_REG0_STS_DC_OK); // wait until the DCDC output stabilises
the chance that it hangs waiting for a change to complete is reduced. Yesterday, after 2500 resets it got stuck (and the watchdog triggered) just twice.
I do however note that if the test has been running already for a long time the chance of it getting stuck seems to be reduced too - maybe something that is temperature dependent?
I have attached a binary that runs on the MIMXRT1020EVK. If the USB device cable is connected to a hist it will reset each time the USB enumerates (so there is a beep every approx. 2s). When the problem occurs it is noticeable due to the beep stopping for a few seconds (the WDOG is set to 4s).
After each restart there is output on the debug interface (the board's CDC UART connection) which shows the number of resets that have been tested and the overall time of operation:
Hello, world... MIMXRT1020 [Software 508 (1)] <----- 508 SW resets + (1) WDOG reset
Unique ID: 0x65f824a41b2119d2-50000004
01.01.1970 00:21:21 <---- time since the EVK was powered on
Static memory = 0x00000878
OS Heap use = 0x000003d5 from 0x00011000
Initial stack margin 0x0001e5b8
FlexRAM:
2 Code banks [0x00000000..0x0000ffff]
6 Data banks [0x20000000..0x2002ffff]
SPI Flash: ISSI 8MByte IS25LP032A
I will repeat the test on some other EVKs to see whether there is a difference in their reliability with respect to the DCDC configuration.
Regards
Mark
Looks like MIMXRT1060EVK is free of the issue:
Hello, world... MIMXRT1060 [Software 3005] <----------3005 SSW resets counted
Unique ID: 0x65f82946453849d2-500000ff
01.01.1970 02:13:55 <--- in 2hrs 13 minutes
Static memory = 0x000008c8
OS Heap use = 0x000003d5 from 0x0002b000
Initial stack margin 0x00044568
FlexRAM:
2 Code banks [0x00000000..0x0000ffff]
14 Data banks [0x20000000..0x2006ffff]
SPI Flash: ISSI 8MByte IS25LP032A
>3000 sw resets without it hanging on the DCDC configuration.
Looks like MIMXRT1024EVK is free of the issue (although I only tested for about 1 hour)
Hello, world... MIMXRT1024 [Software 1780] <----------1780 SW resets counted
Unique ID: 0x677efb092d3a19d2-50000030
01.01.1970 00:55:22 <--- in 55 minutes
Static memory = 0x00000878
OS Heap use = 0x000003d5 from 0x0000a000
Initial stack margin 0x000255b8
FlexRAM:
2 Code banks [0x00000000..0x0000ffff]
6 Data banks [0x20000000..0x2002ffff]
SPI Flash: Winbond 4MByte W25Q32
MIMXRT1062DVL6B
MIMXRT1062CVL5B
MIMXRT1061CVL5B
Are you a dealer? The prices are ridiculously high. My purchase price is 30% cheaper than yours.
Hi
No, not dealer but developer supplying mainly SW solutions/projects but also with HW backup (like proven standard designs), including processor stocks to ensure rapid production runs.
The parts prices shown are unit prices and in quantity they can be supplied at typically 10% lower than the best distributor price, but priority and best discounts are given to uTasker i.MX RT project users - where MIMXRT1062DVL6B (Q2 2023) can be immediately supplied for around $6 each in quantity.
Regards
Mark
Hi All
I have some more insight into the issue.
This is what happens when everything works as expected:
The top line shows some GPIO changes that help to identify when things occur.
Initially the DC/DC converter has an output value of 1.25V and when the SW reset is executed it ramps down to 1.1V in about 1ms.
The ROM loader runs for about 10ms before the application is started (running in XiP mode), seem by the GPIO going to '1'.
The DCDC converter value is (re)programmed and the output ramps (with some ripple) up to 1.25V in about 1ms.
The stable flag is detected at the point where the GPIO goes low again and all continues normally.
When it hangs it always does the following:
In thsi case it is seen that the application starts and commands the DCDC value but it never changes and so the flag loop spins forever (GPIO doesn't go low again).
Since WOG3 is being used to monitor this situation it finally resets and recovers as the next time it manages to set the DCDC voltage as expected:
I added this to the DCDC voltage command:
DCDC_REG3 = ((DCDC_REG3 & ~DCDC_REG3_TRG_MASK) | DCDC_REG3_TRG_1_250V); // increase the DCDC voltage from default 1.15V to 1.25V
while ((DCDC_REG3 & DCDC_REG3_TRG_MASK) != DCDC_REG3_TRG_1_250V) {
set_test_output();
DCDC_REG3 = ((DCDC_REG3 & ~DCDC_REG3_TRG_MASK) | DCDC_REG3_TRG_1_250V); // increase the DCDC voltage from default 1.15V to 1.25V
}
but it didn't help (the test output was never set), meaning that the register value was indeed set correctly (could be read back as expected) but the voltage nevertheless doesn't change.
The question therefore remains as to how it can be possible that the DCDC output value doesn't react to the configuration setting?
Regards
Mark