Changing the SLN-VIZNAS-IOT capabilities

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Changing the SLN-VIZNAS-IOT capabilities

376 次查看
DBrongiel
Contributor I

I am looking to expand the capabilities of the SLN-VIZNAS-IOT board. I want to change the parameters of the face detection so the board can recognize something other than faces. Also, I want to add a counter that displays the number of times a registered user is detected. Can someone assist me with this?

0 项奖励
1 回复

369 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi @DBrongiel ,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) I want to change the parameters of face detection so the board can recognize something other than faces.
-- No, I'm afraid it's impossible to do it.
2) Also, I want to add a counter that displays the number of times a registered user is detected. Can someone assist me with this?
-- I already shared my advice in your another question, please check it.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励