Hello ,
i am working on MaaXBoard RT V3 board with MIMXRT1176DVMAA controller for an application of interface with External flash,
I have imported the out of box demo application from github
when i debug the project from MCUXresso IDE i am getting the following error
Awaiting telnet connection to port 3330 ...
GDB nonstop mode enabled
FreeRTOS stack backtrace is disabled in Non-stop mode (use All-stop)
After error Nn(05). Wire ACK Wait in DAP access -
Failed to read address register in DAP - Nn(05). Wire ACK Wait in DAP access
Target error from Write Memory: Em(17). Debug port inaccessible after access at location 0x80000000
GDB stub (C:\nxp\MCUXpressoIDE_11.6.0_8187\ide\plugins\com.nxp.mcuxpresso.tools.bin.win32_11.6.0.202207121507\binaries\crt_emu_cm_redlink) terminating - GDB protocol problem: Pipe has been closed by GDB.
state - running or following reset request - re-read of state failed - rc Nn(05). Wire ACK Fault in DAP access
i have disabled the XIP_EXTERNAL_FLASH preprocessor.below is the screen shot of the preprocessor settings.
below is the screenshot of MCU memory settings
What might be the issue?
Regards
Sanath
Hi
There is a similar issue about ‘Wire ACK Wait in DAP access’ discussed here
Regards
Daniel
Hi,
Any suggestion on above issue will be appreciated .Thank you.
Is it Project settings issue?
Regards
sanath