Booting on FLEXSPI Port A with S26KS512S from MIMXRT685SFVKB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Booting on FLEXSPI Port A with S26KS512S from MIMXRT685SFVKB

559 Views
daiki
Contributor I

I'm having trouble booting.

The ISP pin settings are correct.

 

How do I configure OTP and configure FCB to boot MIMXRT685SFVKB with FLEXSPI Port A using S26KS512S?

Thanks.

Labels (1)
0 Kudos
1 Reply

548 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @daiki ,

   S26KS512S is the hyperflash, and you connect to the flexspi A port.

ISP need to be:

kerryzhou_0-1627873030087.png

Can you try to use the MCUbootUtility tool to connect your board in the ISP mode?

https://github.com/JayHeng/NXP-MCUBootUtility/archive/refs/tags/v3.3.0.zip
the related user manual is:
https://github.com/JayHeng/NXP-MCUBootUtility

Whether the connection will be OK or not?

kerryzhou_1-1627873160079.png

I think, you don't use the OTP at first, just test it at first, whether it works or not, as the option0 and option1 can define the flash type, you can check RT600 UM chapter 41.5.1.5.2 FlexSPI NOR flash config parameters

Best Regards,

Kerry

 

 

 

 

0 Kudos