Blackscreen/Freeze screen on Board with certain bigger aplications

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Blackscreen/Freeze screen on Board with certain bigger aplications

95 Views
RobinS
Contributor I

The Board gets stuck or doesnt even start, when the single screens are a bit bigger (multiple widgets) but the storage of the board is shown to be only 4 percent filled.

Labels (1)
0 Kudos
1 Reply

79 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @RobinS,

Could you provide more details about this issue, like how are you debugging this issue, what version of GUI Guider you are using and if you are basing your project on an example project? The SmartAppliance demo, for example, is a large demo with multiple widgets that takes a considerable amount of storage compared with the rest of the simpler demos. Do you also see this issue when running the SmartApplicance demo on your RT1050?

BR,
Edwin.

0 Kudos