ASSERT ERROR fsl_sd.c 2115

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ASSERT ERROR fsl_sd.c 2115

Jump to solution
2,834 Views
luishs
Senior Contributor I

Hello.
I am testing SDK examples for the evaluation boards with the RT1176 and RT1166. Everything I try with SD card access fails.

The sources are those given as examples in the SDK, I have not modified anything, and the two boards are new recently purchased. I use 8Gb micro SD cards formatted in FAT32.

Attached screenshots of the errors, ASSERT ERROR fsl_sd.c 2115.

ScreenHunter_005.jpgScreenHunter_009.jpgSD_FAIL_RT1176_RT1166_EVK.jpgSD_FATFS_FALLO_.jpgScreenHunter_002.jpgScreenHunter_004.jpg

 

 

0 Kudos
1 Solution
2,730 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thanks for your reply and sharing.
I basically replicate the phenomenon (as the below figure shows).

jeremyzhou_0-1635498346718.png

To improve the decoding performance, you can place the crucial code in the SDRAM instead of QSPI, further, you can use the FFMpeg instead of the OpenH246, as the FFmpeg has a better performance in decode and please refer to the post.

jeremyzhou_1-1635498358503.png

 

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
9 Replies
2,814 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
Before answering your question, I was wondering if you can introduce the testing environment, such as the version of IDE, SDK library, EVK, etc.
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
2,808 Views
luishs
Senior Contributor I

 

Thanks, I already solved the problem.
The problem is that in the example sources of the SDK for programs with SD card, the switch of the SD card is used as Card Detect, but in the EVK evaluation boards for the RT1166 and RT1176, the DAT3 signal is used as Card Detect, so that's why it didn't work. Looking through the sources I already found where the SD card detect system is defined and I changed it. This should be documented in the project's DOC directory file, but it is not.

However, let's see if you can help me with another topic. I am testing the SDK sample sources to play h264 video files, I have tested it with the evaluation boards for the RT1166 and RT1176, and what I see is that the playback of the videos is very slow for a resolution of 800 * 480 and 30fps, it improves a lot with half resolution at 400 * 240 and 24fps, but this is a serious limitation to be able to use it. I was surprised that a microcontroller as powerful as the 1Ghz RT1176 is not able to decode h264 videos in run time to play them at the correct speed at a resolution higher than 400 * 240.

Can you provide me with another example source that works better to play videos with the RT1166 or RT1176 ?, I also tried the example that plays videos from looped JPEG images, but the result is the same, it is very slow.

0 Kudos
2,801 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
I just run the evkmimxrt1170_h264_freertos_cm7 for testing, and in my opinion, the video frame is played smoothly, as the below video shows, the LCD is 720x1280.


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
2,790 Views
luishs
Senior Contributor I

 

No, that is not correct.
The test video that you are using, which is the one suggested in the sources, does NOT have a resolution of 720 * 1280, that is the resolution of the screen. The program always resizes the video to fill the entire screen, even distorting the video's proportions to fit the screen.

That video you have tried probably has a resolution of 360 * 240 or similar, so it looks fluid.

Try to create a video with a higher resolution, for example 800 * 480, and you will see that it plays very slowly. You can convert any video, for example from mp4 to h264, with the ffmpeg utility and test.

Example of using ffmepg:
ffmpeg -i video.mp4  000.h264

0 Kudos
2,775 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thanks for your reply.
Okay, I'll try it later, or you can upload an MP4 video for comparison test.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

 

0 Kudos
2,749 Views
luishs
Senior Contributor I

 

Ok, I have prepared two h264 videos, one of 800*480 30fps and the other of 400*240 24fps. You can download them from this RAR file that I have uploaded to MEGA.

https://mega.nz/file/NIUCRRSb#wzkowDMh6lEVb2AdbdZmDRBlwPpRIZ4wgPyZAqinsjs

It is the same video with different resolution and fps. The 400*240 24fps practically plays at the correct speed, the same speed as the original mp4, but with half resolution and lower fps. The 800*480 30fps video plays much slower, it is the resolution and fps of the original mp4 file.

So it seems the SDK example sources to play h264 videos with RT1166 and RT1176 and also with the sources to play JPG looped as if it were a video, there are limitations in terms of the resolution of the video, at higher resolution or fps, there comes a time when the video plays very slowly. I would say that above 400*240 24fps the playback speed starts to slow down and is no longer useful.

 

ScreenHunter_012.jpg

0 Kudos
2,731 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thanks for your reply and sharing.
I basically replicate the phenomenon (as the below figure shows).

jeremyzhou_0-1635498346718.png

To improve the decoding performance, you can place the crucial code in the SDRAM instead of QSPI, further, you can use the FFMpeg instead of the OpenH246, as the FFmpeg has a better performance in decode and please refer to the post.

jeremyzhou_1-1635498358503.png

 

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
2,711 Views
luishs
Senior Contributor I

Ok, thank you very much for the information.

I opened another case related to MIPI DSI displays, and the SDK sample sources, to play h264 videos and JPEG photos in loop, with EVK RT1166 and RT1176 evaluation boards.

Can you help me ?

My question in particular, is in which specific source file are the MIPI commands to configure the screen, in those example sources that I have mentioned. Since we have other MIPI screens and also the corresponding datasheets of the controller chips for each screen, we only need to know in which source file the screen is configured, to change the commands to those necessary for our other MIPI screens.

 

0 Kudos
2,692 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
1) Can you help me?
-- Of course, please send the case No or link.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------