μSDCard Issues with iMXRT1020

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

μSDCard Issues with iMXRT1020

Jump to solution
405 Views
andrew58210
Contributor II

Hello,

We are having issues with certain μSD cards with our custom board.  The cards seem to fail in the 400kHz clock rate phase or at the first attempt at a higher speed.  It is worth noting we did not appreciate the additional circuitry on the Eval board like the SD0_VSELECT and SD_PWREN.  We did not implement these and thus I believe we need to force the driver to only work in standard speed mode with 3.3V only I/O.  It is not very clear how to do this.  In an attempt to keep it from running in UHS mode we turned off the following.  It is worth noting the cards that don't work on our board do work on the eval board using the SDCARD_FATFS_FREERTOS demo.

FSL_FEATURE_USDHC_HAS_SDR50_MODE

FSL_FEATURE_USDHC_HAS_SDR104_MODE

This did not seem to resolve the issue.  What else might we need to do?  We are ok with running at slower speed 25Mhz and 3.3V I/O if we get it working, but like I said it isn't clear how to force the driver to do this.  Thanks

Labels (2)
0 Kudos
1 Solution
317 Views
andrew58210
Contributor II

Hi Diego,

We did limit the modes to Standard Speed mode and disabled the UHCI related modes since we did not implement the variable I/O voltage.  This did not resolve everything.  We discovered that for some reason the driver and CPU peripheral really needs the "SD CARD POWER SWITCH" to cycle power to the SDcard.  We find this very strange but when we installed the switch on our board and routed "SD_PWREN" to the correct pin in the software, everything started to work just fine.  Without this we had cards failing in the initial 400kHz mode.

View solution in original post

3 Replies
320 Views
diego_charles
NXP TechSupport
NXP TechSupport

Hi @andrew58210 

I hope you are doing great, my apologies for the delayed response. Are you still having the same inquiry, or do you found out something new to aid the troubleshooting of this? Anyway, please allow me to provide you, my response.

I understand that you want to force the SDK driver to work  at desired speed and desired voltage. In the case you want to change SD bus timing please check the below suggestions.

Modifying below macros is ok. 

 

FSL_FEATURE_USDHC_HAS_SDR50_MODE  (0)// in case you do not want 100 MHz
FSL_FEATURE_USDHC_HAS_SDR104_MODE (0) // in case you do not want 200 MHz

 

But you need to check the setup done in the  SDMMCHOST_Init(sdmmchost_t *host) function.

Inside this function the i.MX RT SDMM host specifications are defined. This structure is especially important. So, you could change SD host parameters.

 

    host->capability = (uint32_t)kSDMMCHOST_SupportHighSpeed | (uint32_t)kSDMMCHOST_SupportSuspendResume |
                       (uint32_t)kSDMMCHOST_SupportVoltage3v3 | (uint32_t)kSDMMCHOST_SupportVoltage1v8 |
                       (uint32_t)kSDMMCHOST_SupportVoltage1v2 | (uint32_t)kSDMMCHOST_Support4BitDataWidth |
                       (uint32_t)kSDMMCHOST_SupportDDRMode | (uint32_t)kSDMMCHOST_SupportDetectCardByData3 |
                       (uint32_t)kSDMMCHOST_SupportDetectCardByCD | (uint32_t)kSDMMCHOST_SupportAutoCmd12;

 

The function  SD_SelectBusTiming(sd_card_t *card) is also important. You need to take a closer look at how this function executes, since it will select whether the SD card will work with  SDR104, SR50 or less. 

I hope this could be of any help,

Diego

 

0 Kudos
318 Views
andrew58210
Contributor II

Hi Diego,

We did limit the modes to Standard Speed mode and disabled the UHCI related modes since we did not implement the variable I/O voltage.  This did not resolve everything.  We discovered that for some reason the driver and CPU peripheral really needs the "SD CARD POWER SWITCH" to cycle power to the SDcard.  We find this very strange but when we installed the switch on our board and routed "SD_PWREN" to the correct pin in the software, everything started to work just fine.  Without this we had cards failing in the initial 400kHz mode.

312 Views
diego_charles
NXP TechSupport
NXP TechSupport

Hi @andrew58210 

Thanks for letting me know, I am glad that your application is now working. 

Diego

0 Kudos